CodeWarrior 10.5 does not support the MPC866. Use CodeWarrior 8.8 for software developing and debugging for the MPC866:
See also attached snapshots.
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Does the 8.8 version be able to install in Ubuntu OS?
thank you for reply,
One more suggestion i want regarding suitable JTAG and drivers for SPI, UART and parallel bus for MPC866.
And even can i find drivers for SPI, UART and parallel bus anywhere.
Thank you for the reply sir,
i more suggestion i want, can i know that which is the suitable JTAG for MPC866
search for Code Warrior USBTAP probe
Thank you for the information Mr. Zhang.
It will be helpful for me if you give any suggestion regarding peripheral drivers for MPC866
Sorry for replying later. I have no idea about the probe's driver, however, it seems like that the driver is installed automatically. The information about the Code Warrior USBTAP probe, refer to the link:
BR,
jinyu