Hello All,
Could anybody provide root file system for mpc8569mds? The BSP only provide ram disk file system. I need a JFFS2 image. I tried to build ltib on Ubuntu 10.04 but in vain.
Thanks and regards,
Adeel
Hi,
After installing the packages as you mentioned, I am still getting the same previous error:
[LD] pmm
/usr/bin/ld: skipping incompatible /usr/lib/gcc/i486-linux-gnu/4.4.3/../../../../lib/libpmll.a when searching for -lpmll
/usr/bin/ld: skipping incompatible /usr/lib/../lib/libpmll.a when searching for -lpmll
/usr/bin/ld: skipping incompatible /usr/lib/gcc/i486-linux-gnu/4.4.3/../../../libpmll.a when searching for -lpmll
/usr/bin/ld: skipping incompatible /usr/lib/libpmll.a when searching for -lpmll
/usr/bin/ld: cannot find -lpmll
collect2: ld returned 1 exit status
make[1]: *** [/opt/freescale/ltib/usr/src/rpm/BUILD/pme_tools-1.0.0/bin_i686/pmm] Error 1
make: *** [applications] Error 2
error: Bad exit status from /home/adeel/ltib-mpc8569mds-20101202/tmp/rpm-tmp.M5AS9e (%build)
Any help will be much appreciated!
Adeel
Technical support comment:
What is version of Linux on your PC?
We tested under LTIB BSP under Ubuntu 10.04 and Ubuntu 12.04.
If Ubuntu 12.04 is used, see please the following pages:
(https://community.freescale.com/thread/117194). Load please the ubuntu-ltib-patch.tgz from the following page (https://community.freescale.com/servlet/JiveServlet/downloadBody/93454-102-3-2834/ubuntu-ltib-patch....).
More comment from technical support.
I use Ubuntu 10.04 LTS.
The following patches are installed on the Ubuntu 10.04:
sudo apt-get install autoconf automake libtool gettext x-dev xorg-dev
sudo apt-get install patch g++ rpm zlib1g-dev m4 bison libncurses5-dev libglib2.0-dev gettext build-essential tcl intltool libxml2-dev liborbit2-dev libx11-dev ccache flex uuid-dev liblzo2-dev
sudo apt-get install autoconf automake libtool gettext x-dev xorg-dev patch g++ rpm zlib1g-dev m4 bison libncurses5-dev libglib2.0-dev gettext build-essential tcl intltool libxml2-dev liborbit2-dev libx11-dev ccache flex uuid-dev liblzo2-dev
We do not see any problem if the MPC8569MDS LTIB BSP is built under Ubuntu 10.04.
Lumin,
Did you try with Ubuntu 10.04 64-bit machine? I have an i686 machine:
Linux adeel-desktop 2.6.32-46-generic-pae #107-Ubuntu SMP Fri Mar 22 19:56:07 UTC 2013 i686 GNU/Linux
I have installed pme_tools package after several tries but after that it stuck now on /opt/freescale/ltib/usr/bin/rpm command. There is no /bin folder in ltib directory. I think the build system has problems in installing libraries/folders in /opt/freescale/ltib directory.
The new Yocto project has a root fs build system for mpc8544 boards which also has same e500v2 core as on mpc8569. Could you confirm if the Yocto generated file system will work on mpc8569 boards?
Thanks and regards,
Adeel
This LTIB BSP are tested under Ubuntu 10.04 32-bit, Ubuntu 12.04 32 bit, Ubuntu 12.04 64-bit.
The following pages were used for LTIB building under Ubuntu 64-bit building:
https://community.freescale.com/docs/DOC-93394
https://community.freescale.com/thread/117194
In order to build pme_tools, you need to build the dependence package pme_priv, please select pme_priv in ltib package.
Or use the following commands to deploy pme_priv first.
./ltib -m prep -p pme_priv
./ltib -m scbuild -p pme_priv
./ltib -m scinstall -p pme_priv
./ltib -m scdeploy -p pme_priv
Thanks,
Yiping
Processing: pme_tools
=======================
Build path taken because: directory build, no prebuilt rpm,
Testing network connectivity
OK GPP:
Try pme_tools-1.0.0-a6.tar.gz.md5 from the GPP
http://bitshrine.org/gpp//pme_tools-1.0.0-a6.tar.gz.md5:
2013-07-01 14:23:03 ERROR 404: Not Found.
Try pme_tools-1.0.0-a6.tar.gz from the GPP
http://bitshrine.org/gpp//pme_tools-1.0.0-a6.tar.gz:
2013-07-01 14:23:04 ERROR 404: Not Found.
Can't get: pme_tools-1.0.0-a6.tar.gz at ./ltib line 790.
Died at ./ltib line 1380.
traceback:
main::build_host_rpms:1380
main::host_checks:1435
main:542
Any Idea?
Adeel
Package pme_priv and pme_tools have been provided in MPC8569 ISO MPC8569MDS_20100518_ltib.iso, and when install ltib these all tar balls and related patches will be installed in /opt/freescale/pkgs folder.
How did you install ltib? Do you have the permission to create /opt/freescale/pkgs folder when installing ltib?
This is not the problem of permission since other packages are already installed in /opt/freescale/pkgs and it only complains about pme_tools.
I think my ltib ISO doesn't has pme_tools package. I am using ltib-mpc8569mds-20101202 which is shipped in CD with mpc8569 development board. Could you provide a link to download MPC8569MDS_20100518_ltib.iso ?
Thanks and regards,
Adeel
After mount the BSP ISO, please check whether pkgs folder contains pme_tools packages, if not, please download 8569 BETA BSP from http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_BSP_PPC_85XX.