Maximum speed (Frequency) of the MPC8548 COP interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Maximum speed (Frequency) of the MPC8548 COP interface

792 次查看
louissankoorika
Contributor I

Hi,

Need information of maximum speed (Frequency) of the MPC8548 COP interface  to ensure signal integrity when designing with MPC8548 device on board.

Is it same as the JTAG clock frequency: 33MHz?

Thanks

Louis

0 项奖励
回复
1 回复

743 次查看
ufedor
NXP Employee
NXP Employee

Maximum COP/JTAG external clock frequency is 33 MHz.
Please refer to the MPC8548E PowerQUICC III Integrated Processor Hardware Specifications, 12.2 JTAG AC Electrical Specifications.

0 项奖励
回复