MPC8378

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC8378

1,301 次查看
Anan
Contributor II

Hi,

How much time is required by MPC8378 core to be stable when 1.0V supply is given to the powerpc core. And basically how much delay is required while sequencing supplies between 1.0V and 3.3V for MPC8378.

Thanks and Regards

-Anand


标记 (1)
1 回复

995 次查看
genuap
NXP Employee
NXP Employee

Hopefully you found the power sequencing in section 2 of the HW spec? It's not spec'd as delay - it has to do with the ramp up time. The core voltage has to be at 90% (i.e. 0.9V ) before I/O voltage reaches 10% of it's value.

And as for the 1.0V stability - the requirement is driven by clock and is specified as requirement for reset held low while you have a stable clock (table 11 in the Spec I'm using). The requirement listed there is 32 clocks. So, basically 32 clocks after power is stable and clock is stable, you can release PORESET.

... Paul