MPC8323 FLASH配置

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8323 FLASH配置

Jump to solution
2,542 Views
Zhang_123
Contributor II

目前在使用MPC8323再进行设计,在codewarrior软件NOR FLASH列表里的型号都是镁光的Flash,可以推荐一下非镁光的型号么?要求使用,容量128M及以上;

 

此前选型到ISSI一款NOR FLASH,跟之前在用的IN28F128J3基本参数相同,但内部buffersize比在用的少(32words),想问下codewarrior是否可以自定义flash配置,把buffersize改小?非常感谢!有关于配置和添加Flash新型号的文档资料么?非常感谢!

0 Kudos
Reply
1 Solution
2,515 Views
yipingwang
NXP TechSupport
NXP TechSupport

如果您安装了CodeWarrior for PA 10.5.1, 请参考C:\Freescale\CW_PA_v10.5.1\PA\PA_Tools\FlashToolKit\Documentation\AppNote-FlashProgrammer-PowerArchitecture.pdf 创建新的flash programing算法,添加新的flash设备到CodeWarrior IDE里面。

View solution in original post

0 Kudos
Reply
3 Replies
2,516 Views
yipingwang
NXP TechSupport
NXP TechSupport

如果您安装了CodeWarrior for PA 10.5.1, 请参考C:\Freescale\CW_PA_v10.5.1\PA\PA_Tools\FlashToolKit\Documentation\AppNote-FlashProgrammer-PowerArchitecture.pdf 创建新的flash programing算法,添加新的flash设备到CodeWarrior IDE里面。

0 Kudos
Reply
2,377 Views
Zhang_123
Contributor II

非常感谢您的回复,目前我正在按照文档进行参数配置,但是有些参数不是很明白,想请教下

ISSIFLASH芯片型号为IS29GL128-70DLEB的DEVICE ID对应Word模式和byte模式下各有3个,而MPC8323的配置文件里面看已有的其他型号的ID应该是跟模式(如8M*16*116M*8*2等)一一对应的,即一个模式一个ID号,所以想请教下,device IDMPC8323FLASH配置列表该如何选择?附件是已经填写的参数和对应的ISSI型号的数据手册。请查收,非常感谢!

Zhang_123_0-1693409831093.png

 

0 Kudos
Reply
2,339 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the following.

<organizationcount>3</organizationcount>

   <organization>8Mx16x1</organization>

   <organization>8Mx16x2</organization>

   <organization>8Mx16x4</organization>

   <id> 227E </id>

   <id> 2221 </id>

   <id> 2201 </id>

   <algorithm>amd16x1.elf</algorithm>

   <algorithm>amd16x2.elf</algorithm>

   <algorithm>amd16x4.elf</algorithm>

0 Kudos
Reply