MPC8315E-RDBA I2C flashing issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8315E-RDBA I2C flashing issue

688 Views
eduardbartosh
Contributor II

Hello,

I tried to flash u-boot on my MPC8315E-RDBA Rev C board using kermit on my PC and I2C flasher embedded into the board. Kermit was able to transfer u-boot.bin just fine. However, after that flashing fails with the error "Flash not Erased". Here is the full console output:

------

## DONE binary (kermit) download

Serial Download Done

Flash Init Done

detected flash

...... done

Flash not Erased

The write error has occured and flash cann't be written

--------

I tried different u-boot builds with the same effect.

The DIP switch S3 is in ON-OFF-ON-ON (0100) position as was suggested by flashing instructions.

Can anybody help with this?

Thank you,

Ed

 

0 Kudos
3 Replies

522 Views
eduardbartosh
Contributor II

S4 is in default state - OFF-OFF-OFF-OFF (1111)

Full log:

$ ./cku300.linux-x86_64-db6.0 -l /srv/tftp/mpc8315/reserved/pty -b 115200

C-Kermit 9.0.300 OPEN SOURCE:, 30 Jun 2011, for Linux (64-bit)

Copyright (C) 1985, 2011,

  Trustees of Columbia University in the City of New York.

Type ? or HELP for help.

(/home/ed/mpc-uboot/) C-Kermit>c

Connecting to /srv/tftp/mpc8315/reserved/pty, speed 115200

Escape character: Ctrl-\ (ASCII 28, FS): enabled

Type the escape character followed by C to get back,

or followed by ? to see other options.

----------------------------------------------------

Hello and welcome to I2C BOOTLOADER

## Ready for binary (kermit) download

C-Kermit>SET PREFIXING ALL

C-Kermit>send u-boot.bin 

SF

X to cancel file,  CR to resend current packet

Z to cancel group, A for status report

E to send Error packet, Ctrl-C to quit immediately:

u-boot.bin => U-BOOT.BIN

Size: 317020, Type: binary

    File   Percent       Packet

    Bytes  Done     CPS  Length

   317020  100%    2508       6  [OK]

ZB

C-Kermit>c

Connecting to /srv/tftp/mpc8315/reserved/pty, speed 115200

Escape character: Ctrl-\ (ASCII 28, FS): enabled

Type the escape character followed by C to get back,

or followed by ? to see other options.

----------------------------------------------------

## DONE binary (kermit) download

Serial Download Done

Flash Init Done

detected flash

...... done

Flash not Erased

The write error has occured and flash cann't be written

 

0 Kudos

522 Views
eduardbartosh
Contributor II

Hello,

Any news on this? Did you have time to reproduce the issue?

Regards,

Ed

0 Kudos

522 Views
ufedor
NXP Employee
NXP Employee

Please provide complete log and settings of the S4.

0 Kudos