Hello Freescale community liner
we are usage the MPC8313 chipset
we are create File system
however, we don't LTIB build on ubuntu v12LTS
how about that
**************************************************************
fdj@ubuntu:~/ltib$
fdj@ubuntu:~/ltib$ ./ltib
Don't have HTTP::Request::Common
Don't have LWP::UserAgent
Cannot test proxies, or remote file availability without both
HTTP::Request::Common and LWP::UserAgent
sh: 2: g++: not found
sh: 1: tclsh: not found
ltib cannot be run because one or more of the host packages needed to run it
are either missing, failing, out of date or not in ltib's standard path.
Current the PATH environment is set to:
/opt/ltib/usr/bin:/usr/local/bin:/usr/bin:/bin:/usr/bin/X11:/usr/X11R6/bin
Please correct this problem (e.g. install/upgrade these packages on your host).
If you have your own utilities in non-standard paths, please add an entry
into the .ltibrc file for example:
%path_std
/usr/local/bin:/usr/bin:/bin:/usr/bin/X11:/usr/X11R6/bin:/my/own/exes
Package Minimum ver Installed info
------- ----------- ---------------
libstdc++ 0 not installed or error
gcc-c++ 2.96 not installed or error
zlib-devel 0 not installed or error
rpm 0 not installed or error
rpm-build 0 not installed or error
ncurses-devel 0 not installed or error
m4 0 not installed or error
bison 0 not installed or error
tcl 0 not installed or error
Died at ./ltib line 1508.
traceback:
main::host_checks:1508
main:562
Started: Thu Jun 20 22:04:08 2013
Ended: Thu Jun 20 22:04:08 2013
Elapsed: 0 seconds
VERSION : 13.2.1
CVS_VERSION : $Revision: 1.90 $ (Savannah)
PLATFORM :
GNUTARCH :
TOOLCHAIN :
TOOLCHAIN_CFLAGS :
Build Failed
Exiting on error or interrupt
********************************************************