How to communicate from PC to MPC5566 Through Ethernet....?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to communicate from PC to MPC5566 Through Ethernet....?

1,305件の閲覧回数
thirun
Contributor I

Dear All,

         I'm trying develop firmware for MPC5566 based controller board which has got Ethernet interface, Serial port and External Bus Interface.

My requirement is Need to communicate from GUI application running in PC to Controller Board through Ethernet. So as per my understanding need to set some IP address to Controller board in order to communicate from PC. i'm fail to do so.....

        Please can any one suggest how do i proceed...? or is there any alternate method to communicate from PC....?

   The suggestions are greatly appreciated in advance...

Thanks & Regards

Thiru  N

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

997件の閲覧回数
TomE
Specialist II

Simple answer - run Linux on it. Your CPU and board may not have enough memory for that though.

If you don't want to do that you still need some sort of Operating System that can support a Network Stack.

At a minimum you need reliable Ethernet drivers. These are complex and hard to write, so don't try to write one your self.

Then you need an IP Protocol stack to receive and send raw IP packets. You then need at a minimum a UDP stack. That would allow communication with PCs, but you'd be better off running TCP than UDP.

So you need a complete TCP/IP protocol stack. Start searching for what's available. The "Freescale MQX Real-Time TCP/IP Communication Suite (RTCS)" might suit you.


The modern way for a device to get an IP address is to run DHCP. That's how your PCs get their IP addresses. If you're doing that you don't know what IP address the board is going to get so it will have to "advertise" itself somehow. Avahi (or whatever Apple call it) is a possibility for that. If you want the unit to have a fixed IP address then the protocol stacks all support that somehow, but you'll have to add some sort of "User Interface" to allow that address to be entered and stored.

I've spent years doing the above on a project. That wasn't a good use of my time - the company should have bought something rather than pay me to port and write large slabs of it.

Tom

0 件の賞賛
返信

997件の閲覧回数
thirun
Contributor I

Thanks for your suggestion.....!

Regards

Thiru N

0 件の賞賛
返信