Heat sink/fan for MPC8548E?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Heat sink/fan for MPC8548E?

1,005 次查看
rainer03
Contributor I

Can someone recommend a heat sink w/ fan for MPC8548E? Since the manual says it's not good to clip heat sink to the chip directly, I've been looking for models with push pins @ digikey, but didn't find one with good size for it.

标记 (4)
0 项奖励
回复
3 回复数

741 次查看
lunminliang
NXP Employee
NXP Employee

Please see below technical support comment:

On our MPC8548-based CDS board we use heatsink with fan similar to ATS-57000-C1-R0 (digikey ATS1357-ND).

Actually, when I open digikey site "Thermal - Heat Sinks" seach page and select "Push Pin" as attachment method, I see only one heatsink w/fan - ATS-57000-C1-R0.

0 项奖励
回复

741 次查看
rainer03
Contributor I

Thank you for the input. This one looks huge for the processor, and it has a clip to be installed on the other side of the board, which may affect the placement of components in that area (such as capacitors)... I had been looking for models that can be installed to the board directly, something like aavid

10-6327-01G - heatsinks for BGA Devices

I see some boards have this kind of heat sinks w/ fans installed, but can't find a good one.

0 项奖励
回复

741 次查看
lunminliang
NXP Employee
NXP Employee

After consult with out thermal expert, technical support has the comment:

Our expert suggests looking the following two devices, but unfortunately these devices are not available at digikey, as far as I can see.

Power budget MPC8548E @ 1333/533MHz : 10.8W core + 2.5W IO = 13.3W

http://www.enzotechnology.com/performance/slf_1.pdf

Rth=1.9'C/W

die temperature rise = 13.3W * (0.8 + 1.9) = 36'C Maximum ambient (in case air) temperature = 105'C-36'C = 69'C

http://www.enzotechnology.com/performance/cnb_r1reva.pdf

Rth~1.0'C/W with typical dimetr 40mm, 6CFM fan die temperature rise = 13.3W * (0.8 + 1.0) = 24'C Maximum ambient (in case air) temperature = 105'C-24'C = 80'C

For more information about power budget calculations please enter a Service Request.