Hi,
I have written hdlc driver for freescale mpc8309twr board,and i am getting CRC error on receive and non-octet aligned as well as with the help of bd_status , i am getting length of packet equal to 1 , So where i am doing any mistake.
And at the time of sending packet i am instructing hdlc controller to add CRC ,so even i am getting reply for a packet but lenght with one.
My setup is like that : Router1(mpc8309) ----> modem(v.35 to dsl converter)-------->modem(dsl to v.35 converter)---->Router2(mpc8309)
Your answer is appreciated.
Thanks
Muazzam(india)
Typical reason for "Non-octet aligned frame" error is excessive noise on clock input, this is used to sample incoming data. Please check if input clock waveform is correct and clock source output impedance is matched with trace impedance.
Have a great day,
Alexander
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks Alexander,
But when my device is connected to slave mode modem (which gives me clock tx and rx both) then its working fine .
what happens when we connect with Master mode modem.
Basically in CRO i observed ,that i am getting distorted RX input clock in Master mode modem but very clear input clock in slave mode.
And also tested modems in tester and found modem correct.
So what kind of circuit may distort the signal?.
Thanks
Muazzam(india)
Hi alex,
I have changed clock number ,i.e RXLCK =14 for UCC5 in mpc8309 and TXCLK =13,so now i just reversed and it's working .
So my doubt is why d i need to interchange the clock numbers in UCC.Is it one kind of bug in MPC8309 Processor ?.
Thanks
Muazzam(india)
No alex , all connections are correct ,recently i seen in revision 1 of mpc8309RM manual they have mentioned that clock numbers have to interchanged.
Alex if you can tell ,diiferent then HDLC, Why do we need to change the base address of IMMRBAR from FF40_0000 to e000_0000 in init.cfg file which is given by freescale?
Thanks
Muazzam(india)
Yes, you are right. I usually assume customers use most recent revisions of of our documents.
Internal space can be moved from its default position to any other place, if necessary. This is done by writing to IMMRBAR. Usually, IMMR is moved because upper part of memory is used for NOR flash, however this depends on flash size, so - up to designer.