DRIVERS AND JTAG FOR MPC866

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DRIVERS AND JTAG FOR MPC866

998件の閲覧回数
skchethan123
Contributor I

I am using MPC866 in which I have to work with SPI, UART and parallel bus. So can i know that where i can find the drivers for those peripherals. And i want to know which all the supported JTAG for MPC866 

ラベル(3)
0 件の賞賛
3 返答(返信)

843件の閲覧回数
Pavel
NXP Employee
NXP Employee

See simple program examples in the attached file.

If there is a problem for .zip or 7z file loading, create please technical case:

https://community.nxp.com/thread/381898


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

843件の閲覧回数
Pavel
NXP Employee
NXP Employee

See simple program examples in the attached file.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

843件の閲覧回数
skchethan123
Contributor I

sorry Mr. Pavel I did not any attachments.

0 件の賞賛