Cause for damaging 5v rail in MWCT1013 EVK.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cause for damaging 5v rail in MWCT1013 EVK.

1,091 Views
JagirMehta
Contributor II

Hello,

I am using MWCT1013A MP-A9 EVK for a wireless charging project.

I was using it i debug mode & suddenly EVK went power OFF. By checkng HW components, I found that the 5V rail was damaged.

 

Is any firmware malfunction can damage MWCT1013 EVK ?

 

0 Kudos
4 Replies

1,084 Views
JagirMehta
Contributor II

Adding few more queries to the original post.

 

Can any firmware modification damage the 5v rail in EVK ?

Does EVK has any kind of hardware protection for it ?

0 Kudos

1,081 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport
 

Dear Jagir Mehta,

I think the answer is Yes that the inappropriate software even debugging can leads to the board damage.
For example, you set up the PWM signals which drive the H bridge, if the top Mosfet and bottom Mosfet turn on at the same time, the rail voltage will be short to GND, the power supply will be damaged.

BTW, the in appropriate debugging may damage the board with the same reason.

There is a bit to enable the PWM to continue to output or disabled in debug state.

xiangjun_rong_1-1627529962672.png

 


Hope it can help you.

BR

XiangJun Rong

0 Kudos

1,077 Views
JagirMehta
Contributor II

Thanks XinagJun,

 

It does solve my query but I have few doubts here.

In my firmware, I take reference of "WCT-15WTXAUTO_V4.1" example firmware received from NXP.

I did not do any modification peripheral driver files(PWM.c /.h & hal.c /.h). I have modified the main.c file as per my use.

 

Does any malfunctions in main.c file can harm EVK ?

I have used 12v power supply which i received along with MWCT1013A MP-A9 EVK.

Can the power supply damage in debug mode ?

0 Kudos

959 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

If you do want to debug the code, I suggest you clear DBGEN bit in the control2 register.

But I do not suggest you set up a break point and debug the code, if the PWM signals still drive the MOSFET, the board maybe damaged, because the feedback loop is invalid when you stop at break point.

You can run the code continuously and output message via uart.

Hope it can help you

BR

XiangJun Rong

0 Kudos