Can MPC8378 and T1014 share the same JTAG debug tool(LA-7699)?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can MPC8378 and T1014 share the same JTAG debug tool(LA-7699)?

775 次查看
jun_b_zhang
Contributor I

Hi,

Can MPC8378 and T1014 share the same JTAG debug tool(LA-7699)?

MPC8378 belong to PowerQUICC, and T1014 belong to QorlQ.

BR/Jun Zhang

0 项奖励
回复
1 回复

677 次查看
alexander_yakov
NXP Employee
NXP Employee

MPC8378 and T1014 have the same type debug interface and debug interface header, so theoretically they can use the same debug probe. For example, in case of our CodeWarrior TAP both these processors will use the same debug probe tip.

For LA-7699 support please contact product vendor Lauterbach  support@lauterbach.com


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复