As for MPC8377ECVRALGA, can it be set up the SATA test model? We need to issue LFTP, MFTP, and HFTP formats to facilitate the SATA conformance testing.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

As for MPC8377ECVRALGA, can it be set up the SATA test model? We need to issue LFTP, MFTP, and HFTP formats to facilitate the SATA conformance testing.

490 次查看
charlesfu
Contributor I

As for MPC8377ECVRALGA, can it be set up the SATA test model? We need to issue LFTP, MFTP, and HFTP formats to facilitate the SATA conformance testing.

0 项奖励
1 回复

393 次查看
alexander_yakov
NXP Employee
NXP Employee

The test pattern for HFTP,MFTP,LFTP,LBP are generated by external signal generators and sent to the device under test for BIST-L and other BIST modes during SATA compliance test.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励