MPC8308 Clocking Specific FAQs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC8308 Clocking Specific FAQs

MPC8308 Clocking Specific FAQs

For MPC8308 package, which is the GTX clock pin for TSEC1 and TSEC2?

According to the MPC8308 ballmap, V21 is the GTX clock pin of TSEC1 and T19 is the GTX clock pin of TSEC2.


Can a spread spectrum clock be used for the 66.66 Mhz DDR clock of the MPC8308? If so what percentage spread is allowed and what modulation frequency?

Yes, a spread spectrum clock can be used for 66.66 Mhz DDR clock. Please refer to below table for details:

Spread Spectrum Clock Source Recommendations

Parameter Min Max Unit Frequency modulation — 60 kHz Frequency spread — 1.0  %



ラベル(1)
評価なし
バージョン履歴
最終更新日:
‎07-31-2012 09:41 AM
更新者: