TEA2096-The no-load power test is too high

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

TEA2096-The no-load power test is too high

601 次查看
jack_li
Contributor I

The no-load power test is too high,

The impedance of GATE pin (1 pin/8 pins) to ground (2 pins) is significantly low。

 

The no-load power during normal product testing is 0.3-0.4W,

Defective product testing power 0.7W-1W。

Infrared thermometer product ,with a defect rate of 16%

TEA2096.png

0 项奖励
回复
3 回复数

590 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Jack,

how many boards have you tested? Have you tested to replace a TEA2096T from the board, which passed the test to a board, which hasn't passed the test? And vise versa? If yes, which board is now not passing the test? 

Please confirm the source of the TEA2096T components. Have you purchased all of them from one of our authorized distributors? Please state the name of the distributor.

With Best Regards,

Jozef

0 项奖励
回复

585 次查看
jack_li
Contributor I

180 pieces were tested, of which 29 had abnormal no-load power. The supply agent is DIGIKEY。

 

Replace the TEA2096 on the board that passed the test with the board that failed the test, and the test result is still unqualified.

 

TEA2096 is abnormal. When replaced with a board that passed the test or failed the test, the test results are both abnormal.

 

0 项奖励
回复

578 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Jack,

I see you have created a case #00579623 with a very same question. Let's please continue in the case. I will answer you there.

With Best Regards,

Jozef

0 项奖励
回复