Good morning,
We are using the s32k144 microcontroller connected to the MC33664 adapter as hardware and the MC33771C as BMS together with the monitoring sample program. We are also using a 100uOhm shunt resistor.
When measuring the values in the program with the "domeasuraments" function, it reads the voltage values correctly but the Isense values are always 0. We also activate the Isense measures enable bit in the SYS_CFG1 register. Could you tell us what the problem could be?
Thanks in advance!
解決済! 解決策の投稿を見る。
Hello David,
You are correct, the I_MEAS_EN bit from the SYS_CFG1 register enables or disables current measurement (disabled by default).
The BCC_Meas_GetIsenseVoltage should be useful for you as it reads the ISENSE measurement and converts it to [μV].
Could you please share your ISENSE pins configuration?
Hello David,
I hope all is great with you. Thank you for using the NXP communities.
Could you please share more details about your design? I mean, are you using an evaluation board? What is the project or libraries used in your project?
Regards,
David
We are using as hardware a board made up of the s32k144, the MC33664_sds and the MC33771C.We are also using a rshunt of 100uOhms.
About the software we are using the BCC_S32K144_Monitoring program. We change the initialization of the SYS_CFG1[ I_MEAS_EN]=1. So we initialize the SYS_CFG1 register with the 0x1201 value, I think that is correct.
For getting the voltage of the cells we use the BCC_Meas_GetCellVoltages function and we receive the correct values. But when measuring the current value and we use the BCC_Meas_GetIsenseVoltage function we only receive a 0.
Measuring with a multimeter we know that between the ISENSE+ and ISENSE- pins there is 0.5mV so the value of the current should not be 0.
I attach you the main.c to see if you see any errors in the main functions.
Thanks in advance!
Hello David,
You are correct, the I_MEAS_EN bit from the SYS_CFG1 register enables or disables current measurement (disabled by default).
The BCC_Meas_GetIsenseVoltage should be useful for you as it reads the ISENSE measurement and converts it to [μV].
Could you please share your ISENSE pins configuration?
Hello again,
The problem was that we were sending the wrong value to SYS_CF1 so we were not enabling the I_MEAS_EN
Thank you!