Hi NXP community,
I'm struggling with basic communication on a PCA9745B. Reading MODEs 1 and 2 works fine, and I get 0 and 1 as outputs, respectively.
However, anything beyond that gets... strange. For example, reading register 02h (LEDOUT0) after either a RESET or power down/power up gives FFh; it should be AAh, if I understand the defaults correctly. Even stranger, writing AAh to the LEDOUT0 register followed by a read gives 0. If I read again, with no changes, I again get FFh. I have confirmed that all four signals (CS/SCLK/MOSI/MISO) act as they should with an oscilloscope.
Commands look like this:
send_SPI([0b00000101,0b11111111]) #set up to read register 10
send_SPI([0b11111111,0b11111111]) #read out result
printed result: [0,FFh]
send_SPI([0b00000100,0b10101010]) #wire 10 to LED0 through LED 3
send_SPI([0b00000101,0b11111111]) #set up to read register 10
test = send_SPI([0b11111111,0b11111111])
printed result: [0,0]
send_SPI([0b00000101,0b11111111]) #set up to read register 10
test = send_SPI([0b11111111,0b11111111])
printed result: [0,FFh]
Pins:
1) R = 910Ohms (to ground)
2) gnd
3) MISO
4) CS
5) gnd
6) Green LED cathode
7) NC
8) NC
9) NC
10) gnd
11) NC
12) NC
13) NC
14) NC
15) NC
16) NC
17) NC
18) NC
19) gnd
20) NC
21) NC
22) NC
23) NC
24) gnd
25) 10k pull up resistor to +5V
26) SCLK
27) MOSI
28) +5V
Any ideas why this might be happening? I'm happy to share scope readings, code, diagrams, etc. if any additional information would be useful. Thank you in advance!
Cheers,
Dan
I resolved my own issue. For anyone who runs into something similar in the future, the likely culprit is a bad chip (in my case, caused by my own destruction). I had soldered this chip to a breakout board and discovered a small amount of light coming from an LED when PWMall was 0. It seems that I hadn't cleaned the board well enough and some flux offered a current pathway to some of the comm pins. Unfortunately, this meant that the comm pins had been exposed to +10V (the negative side of my LEDs), and likely damaged them as this is well above their voltage tolerance.
Good luck to anyone else struggling with a similar topic! And thanks to NXP for making this chip; the SPI integration and external reference resistor make this chip leagues ahead of others for our application.