MML09212H - Minimum Supply Voltage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MML09212H - Minimum Supply Voltage

727 Views
ricardopereira
Contributor I

Hi, 

What's the minimum supply voltage for the MML09212H? If I power it with 4.5V for exemple, should I expect a big difference in terms of performance?

Thank you,

Kind regards.

0 Kudos
1 Reply

698 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

It is not recommended to supply the MML09212H with a different voltage than 5.0V as this device is only characterized to operate with this voltage supply level.

 

If a different voltage is used, NXP cannot warranty the proper performance of the device.


Have a great day,
Jose

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos