MC34VR5100A2EP compatibility with LX2160A PMBus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC34VR5100A2EP compatibility with LX2160A PMBus

889 Views
Miguel-Avina
Contributor IV

Hi,

Our customer wants clarification about the compatibility of the MC34VR5100A2EP PMIC with the LX2160A PMBus. Specifically, their question is the following:

Will the NXP PMBus driver work with this?  Can the slope (m) be changed to a different value based on Read or Write.

 

Using Direct Mode

VOUT_COMMAND

R=0

m=500

b=0

 

READ_VOUT

R=0

m=800

b=0

 

For VOUT_COMMAND

MiguelAvina_0-1658343842936.png

 

For READ_VOUT

MiguelAvina_1-1658343842941.png

 

MiguelAvina_2-1658343842953.png

Thank you

Tags (1)
0 Kudos
Reply
3 Replies

857 Views
Miguel-Avina
Contributor IV

Hi, there was a misunderstanding with this request. Please see clarification from the customer below:

"

My question is in regards to the LX2160A PMBus driver capabilities when using PMBus Direct VOUT_MODE.

I'm looking to see how the driver deals with the coefficients, m, b & R.  Are they fixed during set up or can they be changed on the fly?  I want to verify the selected power supply is compatible.

Attached is a page from the PMBus Protocol Spec.  I haven't found anything in the NXP documentation that explains the PMBs operation.  

Also, this from the LX2160A datasheet

MiguelAvina_0-1658754788243.png

How does the value stored in the Fuse Status Register get configured to a format usable by a PMBus device and get transferred?

"

Kind regards,

0 Kudos
Reply

856 Views
guoweisun
NXP TechSupport
NXP TechSupport

Unfortunately for the  LX2160A  part questions you need submit ticket to  LX2160A  support team.

Here only support the PMIC side questions.

Home (nxp.com)

0 Kudos
Reply

876 Views
guoweisun
NXP TechSupport
NXP TechSupport

Do you mean the DVS speed selection for SWx of VR5100?

If yes,it can be changed by setting as below picture:

guoweisun_0-1658383690262.png

 

0 Kudos
Reply