FS26 Bad WD refresh, can't enter normal mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS26 Bad WD refresh, can't enter normal mode

2,473 Views
xflong
Contributor III

Hi,

When I used S32K3X4EVB-Q257 to test the function of FS26, I found that Watchdog could not refresh correctly and could not enter the normal mode. When leaving the debug mode, the development board will reset. The FS26_VDEBUG is configured as the default state, and the connectors J685 and J686 are both 1-2.
Attached is my S32DS project. Thanks.

0 Kudos
Reply
3 Replies

2,450 Views
guoweisun
NXP TechSupport
NXP TechSupport

Fs26 has Challenger watchdog and Simple watchdog, please check your SBC which one it has.

For the WD refresh step please read datasheet page182.

2,398 Views
xflong
Contributor III

Thank you for answering my question.

I checked the model of the chip on the development board and changed the watchdog refresh type. Now I can feed the dog correctly. But there are two problems:

1. In normal mode,  The return value eReturnValue of functions such as Sbc_ fs26_ WdRefresh() and Sbc_ fs26_FsxbRelease() may not be equal to E_ OK。 But the chip can work correctly. Why?
2. In the watchdog drive configuration, there is an External watchdog. How do you understand External watchdog?

0 Kudos
Reply

2,373 Views
guoweisun
NXP TechSupport
NXP TechSupport

For other topic I suggest you submit ticket from link:

Home (nxp.com)

0 Kudos
Reply