hello experts
i am new to dts and have a question
in dts file local-mac-address is all zero
but when kernel boots up there are valid mac-address which is set by u-boot's ethaddr variable
i wonder who changes local-mac-address using u-boot's ethaddr variable
before boot , in u-boot i use fdt command and printed dts and local-mac-address are all zero
so i think in kernel bootup process , some process change local-mac-address by using u-boot bdinfo
am i wrong ?
any infomation is welcome
thank you
已解决! 转到解答。
u-Boot performs multiple FDT fixups before passing it to the kernel. local-mac-address is one of the properties that are automatically updated
according to the current configuration. See common/fdt_support.c
Have a great day
Platon
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
u-Boot performs multiple FDT fixups before passing it to the kernel. local-mac-address is one of the properties that are automatically updated
according to the current configuration. See common/fdt_support.c
Have a great day
Platon
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------