the err shows that:
ss@ubuntu:~/shanyf/P4080-PCIE-SDK-1.0-05-03-2012/ltib-e500mc-20110415$ ./ltib
Installing host support packages.
This only needs to be done once per host, but may take up to
an hour to complete ...
If an error occurs, a log file with the full output may be found in:
/home/shanyf/shanyf/P4080-PCIE-SDK-1.0-05-03-2012/ltib-e500mc-20110415/host_config.log
Exiting on error or interrupt
Please see >> /home/shanyf/shanyf/P4080-PCIE-SDK-1.0-05-03-2012/ltib-e500mc-20110415/host_config.log for details
the host_config.log shows that:
rpmdb: --force-debian: unknown option
Died at ./ltib line 2339.
traceback:
main::setup_rpmdb:2339
main::check_rpm_setup:2403
main::host_checks:1424
main:543
Started: Thu Jul 16 18:54:40 2015
Ended: Thu Jul 16 18:54:41 2015
Elapsed: 1 seconds
help me,what should i do ,thanks
This question is frequently asked, for example please look this topic:
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------