qoriq ddr3 with ECC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

qoriq ddr3 with ECC

359 Views
jagxin
Contributor III

Hello everyone

             If we are using ddr3 with ECC where should the chip placed in the daisy chain first from the controller  in between on the last near to termination

if we place first on the daisy chain termination is very far and SI is not that good

whether more care is required for ECC or it Can de given least importance and can be placed first on the Daisy chain

regards

AGXIN.J

Labels (1)
0 Kudos
1 Reply

225 Views
Bulat
NXP Employee
NXP Employee

It does not matter where the ECC chip is placed in the fly-by chain, you can put it first, last or somewhere in between. Note for example that typical DDR3 DIMM has ECC chip in the middle.

Regards,

Bulat

0 Kudos