how can i use 4K-page nand (MT29F8G08ABACAWP) in P1020/P1011

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how can i use 4K-page nand (MT29F8G08ABACAWP) in P1020/P1011

825件の閲覧回数
hyoungkikim
Contributor III

hello experts

CPU is P1020/P1011  and a borad was  used a few years without problems

kernel and u-boot are from SDK 1.8

this time  i have to install 1GB nand  so i  plan to  use  MT29F8G08A instead of MT29F1G08 which  was installed on the board

i read a user guide ann it said  it can interface a small and a large nand , and the large nand is 2K-page device

how could i interface 4K-page nand with FCM   ?

thank you for your advices

ラベル(2)
0 件の賞賛
1 返信

714件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

In u-boot source code include/configs/p1_p2_rdb_pc.h, please configure ELBC  BR and OR as the following.

#define CONFIG_SYS_NAND_BR_PRELIM (BR_PHYS_ADDR(CONFIG_SYS_NAND_BASE_PHYS) \
        | (2<<BR_DECC_SHIFT)    /* Use HW ECC */ \
        | BR_PS_8       /* Port Size = 8 bit */ \
        | BR_MS_FCM     /* MSEL = FCM */ \
        | BR_V) /* valid */
#if defined(CONFIG_P1020RDB_PD)
#define CONFIG_SYS_NAND_OR_PRELIM       (0xFFFC0000  /* length 256K */ \
        | OR_FCM_PGS    /* Large Page*/ \
        | OR_FCM_CSCT \
        | OR_FCM_CST \
        | OR_FCM_CHT \
        | OR_FCM_SCY_1 \
        | OR_FCM_TRLX \
        | OR_FCM_EHTR)
#else

0 件の賞賛