fm2-gb0 ethernet port does not work properly on P4080DS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

fm2-gb0 ethernet port does not work properly on P4080DS

840件の閲覧回数
sharathchandra
Contributor II

Hi,

 

On my P4080Ds board, I am trying to use fm2-gb0 ethernet port. But it does no look like working properly, as it gives errors like Error FD Status and Invalid Enqueue State.

This is the same with other fm2 ports.

I am using rcw_2sgmii_1500mhz_rev3.bin.

 

My dmesg shows the following information:

root@p4080ds:/usr/etc# dmesg

[    1.004979] mpc-i2c ffe119000.i2c: timeout 1000000 us

[    1.008932] mpc-i2c ffe119100.i2c: timeout 1000000 us

[    1.014102] Freescale(R) MPC85xx EDAC driver, (C) 2006 Montavista Software

[    1.020313] mpc85xx_mc_err_probe: No ECC DIMMs discovered

[    1.024440] mpc85xx_mc_err_probe: No ECC DIMMs discovered

[    1.029764] sdhci: Secure Digital Host Controller Interface driver

[    1.034638] sdhci: Copyright(c) Pierre Ossman

[    1.037684] sdhci-pltfm: SDHCI platform and OF driver helper

[    1.064854] mmc0: SDHCI controller on ffe114000.sdhc [ffe114000.sdhc] using DMA

[    1.072337] platform caam_qi.0: Linux CAAM Queue I/F driver initialised

[    1.077740] caam ffe300000.crypto: device ID = 0x0a10030000000000 (Era 1)

[    1.083226] caam ffe300000.crypto: job rings = 4, qi = 1

[    1.088362] authenc-hmac-md5-cbc-aes-caam needs Era 2 or higher but SEC is Era 1, skipping it

[    1.095591] authenc-hmac-sha1-cbc-aes-caam needs Era 2 or higher but SEC is Era 1, skipping it

[    1.102898] authenc-hmac-sha224-cbc-aes-caam needs Era 2 or higher but SEC is Era 1, skipping it

[    1.110371] authenc-hmac-sha256-cbc-aes-caam needs Era 2 or higher but SEC is Era 1, skipping it

[    1.117849] authenc-hmac-sha384-cbc-aes-caam needs Era 2 or higher but SEC is Era 1, skipping it

[    1.125328] authenc-hmac-sha512-cbc-aes-caam needs Era 2 or higher but SEC is Era 1, skipping it

[    1.132807] authenc-hmac-md5-cbc-des3_ede-caam needs Era 2 or higher but SEC is Era 1, skipping it

[    1.140460] authenc-hmac-sha1-cbc-des3_ede-caam needs Era 2 or higher but SEC is Era 1, skipping it

[    1.148200] authenc-hmac-sha224-cbc-des3_ede-caam needs Era 2 or higher but SEC is Era 1, skipping it

[    1.156114] authenc-hmac-sha256-cbc-des3_ede-caam needs Era 2 or higher but SEC is Era 1, skipping it

[    1.164027] authenc-hmac-sha384-cbc-des3_ede-caam needs Era 2 or higher but SEC is Era 1, skipping it

[    1.171941] authenc-hmac-sha512-cbc-des3_ede-caam needs Era 2 or higher but SEC is Era 1, skipping it

[    1.179854] authenc-hmac-md5-cbc-des-caam needs Era 2 or higher but SEC is Era 1, skipping it

[    1.187072] authenc-hmac-sha1-cbc-des-caam needs Era 2 or higher but SEC is Era 1, skipping it

[    1.194378] authenc-hmac-sha224-cbc-des-caam needs Era 2 or higher but SEC is Era 1, skipping it

[    1.201857] authenc-hmac-sha256-cbc-des-caam needs Era 2 or higher but SEC is Era 1, skipping it

[    1.209336] authenc-hmac-sha384-cbc-des-caam needs Era 2 or higher but SEC is Era 1, skipping it

[    1.216814] authenc-hmac-sha512-cbc-des-caam needs Era 2 or higher but SEC is Era 1, skipping it

[    1.216825] mmc0: new high speed SDHC card at address aaaa

[    1.217039] mmcblk0: mmc0:aaaa SU04G 3.69 GiB

[    1.231585] rfc4106-gcm-aes-caam needs Era 2 or higher but SEC is Era 1, skipping it

[    1.238023] rfc4543-gcm-aes-caam needs Era 3 or higher but SEC is Era 1, skipping it

[    1.244457] tls10-hmac-sha1-cbc-aes-caam needs Era 2 or higher but SEC is Era 1, skipping it

[    1.251589] gcm-aes-caam needs Era 2 or higher but SEC is Era 1, skipping it

[    1.251611]  mmcblk0: p1 < p5 >

[    1.259152] cbc-aes-caam needs Era 2 or higher but SEC is Era 1, skipping it

[    1.264889] cbc-3des-caam needs Era 2 or higher but SEC is Era 1, skipping it

[    1.270712] cbc-des-caam needs Era 2 or higher but SEC is Era 1, skipping it

[    1.276447] caam algorithms registered in /proc/crypto

[    1.282768] caam_jr ffe301000.jr: registering rng-caam

[    1.287306] caam ffe300000.crypto: fsl,sec-v4.0 algorithms registered in /proc/crypto

[    1.293961] platform caam_qi.0: authenc-hmac-md5-cbc-aes-caam-qi needs Era 2 or higher but SEC is Era 1, skipping it

[    1.303176] platform caam_qi.0: authenc-hmac-sha1-cbc-aes-caam-qi needs Era 2 or higher but SEC is Era 1, skipping it

[    1.312474] platform caam_qi.0: authenc-hmac-sha224-cbc-aes-caam-qi needs Era 2 or higher but SEC is Era 1, skipping it

[    1.321946] platform caam_qi.0: authenc-hmac-sha256-cbc-aes-caam-qi needs Era 2 or higher but SEC is Era 1, skipping it

[    1.331418] platform caam_qi.0: authenc-hmac-sha384-cbc-aes-caam-qi needs Era 2 or higher but SEC is Era 1, skipping it

[    1.340889] platform caam_qi.0: authenc-hmac-sha512-cbc-aes-caam-qi needs Era 2 or higher but SEC is Era 1, skipping it

[    1.350360] platform caam_qi.0: authenc-hmac-md5-cbc-des3_ede-caam-qi needs Era 2 or higher but SEC is Era 1, skipping it

[    1.360005] platform caam_qi.0: authenc-hmac-sha1-cbc-des3_ede-caam-qi needs Era 2 or higher but SEC is Era 1, skipping it

[    1.369740] platform caam_qi.0: authenc-hmac-sha224-cbc-des3_ede-caam-qi needs Era 2 or higher but SEC is Era 1, skipping it

[    1.379647] platform caam_qi.0: authenc-hmac-sha256-cbc-des3_ede-caam-qi needs Era 2 or higher but SEC is Era 1, skipping it

[    1.389552] platform caam_qi.0: authenc-hmac-sha384-cbc-des3_ede-caam-qi needs Era 2 or higher but SEC is Era 1, skipping it

[    1.399458] platform caam_qi.0: authenc-hmac-sha512-cbc-des3_ede-caam-qi needs Era 2 or higher but SEC is Era 1, skipping it

[    1.409364] platform caam_qi.0: authenc-hmac-md5-cbc-des-caam-qi needs Era 2 or higher but SEC is Era 1, skipping it

[    1.418574] platform caam_qi.0: authenc-hmac-sha1-cbc-des-caam-qi needs Era 2 or higher but SEC is Era 1, skipping it

[    1.427872] platform caam_qi.0: authenc-hmac-sha224-cbc-des-caam-qi needs Era 2 or higher but SEC is Era 1, skipping it

[    1.437343] platform caam_qi.0: authenc-hmac-sha256-cbc-des-caam-qi needs Era 2 or higher but SEC is Era 1, skipping it

[    1.446815] platform caam_qi.0: authenc-hmac-sha384-cbc-des-caam-qi needs Era 2 or higher but SEC is Era 1, skipping it

[    1.456286] platform caam_qi.0: authenc-hmac-sha512-cbc-des-caam-qi needs Era 2 or higher but SEC is Era 1, skipping it

[    1.465757] platform caam_qi.0: tls10-hmac-sha1-cbc-aes-caam-qi needs Era 2 or higher but SEC is Era 1, skipping it

[    1.475721] Freescale USDPAA process driver

[    1.478701] Freescale USDPAA process IRQ driver

[    1.482523] fsl-pme ffe316000.pme: ver: 0x00100201

[    1.486217] Freescale pme2 db driver

[    1.488573] Freescale pme2 scan driver

[    1.491099] fsl-pme2-scan: device pme_scan registered

[    1.495064] Freescale hypervisor management driver

[    1.498578] fsl-hv: no hypervisor found

[    1.501105] oprofile: using ppc/e500mc performance monitoring.

[    1.501218] ipip: IPv4 over IPv4 tunneling driver

[    1.504937] TCP: cubic registered

[    1.506948] Initializing XFRM netlink socket

[    1.509965] NET: Registered protocol family 10

[    1.513523] sit: IPv6 over IPv4 tunneling driver

[    1.517172] NET: Registered protocol family 17

[    1.520322] NET: Registered protocol family 15

[    1.523474] 8021q: 802.1Q VLAN Support v1.8

[    1.526363] Key type dns_resolver registered

[    1.529961] libphy: mdio_mux: probed

[    1.532533] libphy: mdio_mux: probed

[    1.535650] mdio-mux-gpio mdio-mux-emi1.14: Version 1.0

[    1.539665] fsl_dpa_macless: FSL DPAA MACless Ethernet driver ()

[    1.544600] fsl_dpa_generic: FSL DPAA Generic Ethernet driver ()

[    1.550318] rtc-ds3232 0-0068: setting system clock to 2015-03-30 13:57:06 UTC (1427723826)

[    1.557514] Waiting 5 sec before mounting root device...

[    2.793874] ata1: SATA link up 3.0 Gbps (SStatus 123 SControl 0)

[    2.799487] ata1.00: ATA-8: WDC WD5000AAKX-22ERMA0, 17.01H17, max UDMA/133

[    2.805065] ata1.00: 976773168 sectors, multi 0: LBA48 NCQ (depth 31/32)

[    2.811419] ata1.00: configured for UDMA/100

[    2.814551] scsi 0:0:0:0: Direct-Access     ATA      WDC WD5000AAKX-2 17.0 PQ: 0 ANSI: 5

[    2.821729] sd 0:0:0:0: [sda] 976773168 512-byte logical blocks: (500 GB/465 GiB)

[    2.828010] sd 0:0:0:0: [sda] Write Protect is off

[    2.831499] sd 0:0:0:0: [sda] Mode Sense: 00 3a 00 00

[    2.831565] sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA

[    2.832866] sd 0:0:0:0: Attached scsi generic sg0 type 0

[    3.277745]  sda: unknown partition table

[    3.280830] sd 0:0:0:0: [sda] Attached SCSI disk

[    4.964871] ata2: SATA link up 1.5 Gbps (SStatus 113 SControl 0)

[    4.972811] ata2.00: ATAPI: ATAPI   iHAS124   E, 4L06, max UDMA/100

[    4.981507] ata2.00: configured for UDMA/100

[    4.985624] scsi 1:0:0:0: CD-ROM            ATAPI    iHAS124   E      4L06 PQ: 0 ANSI: 5

[    4.995271] sr0: scsi3-mmc drive: 48x/48x writer dvd-ram cd/rw xa/form2 cdda tray

[    5.001452] cdrom: Uniform CD-ROM driver Revision: 3.20

[    5.005605] sr 1:0:0:0: Attached scsi CD-ROM sr0

[    5.005792] sr 1:0:0:0: Attached scsi generic sg1 type 5

[    6.566159] EXT2-fs (mmcblk0p5): warning: mounting unchecked fs, running e2fsck is recommended

[    6.576528] VFS: Mounted root (ext2 filesystem) on device 179:5.

[    6.582771] devtmpfs: mounted

[    6.584598] Freeing unused kernel memory: 272K (c084c000 - c0890000)

[    7.196341] udevd[1081]: starting version 182

[    8.543432] Installing knfsd (copyright (C) 1996 okir@monad.swb.de).

[ 1270.901903] EXT2-fs (mmcblk0p5): error: ext2_lookup: deleted inode referenced: 88707

[ 1305.524784] EXT2-fs (mmcblk0p5): error: ext2_lookup: deleted inode referenced: 88707

[ 1846.382932] Qman ErrInt: Invalid Enqueue State

[ 1846.386743] Qman ErrInt: DCP id 1

[ 1846.390130] Qman ErrInt: ecir.fqid 0xa0a

[ 1847.382272] Qman ErrInt: Invalid Enqueue State

[ 1847.385404] Qman ErrInt: DCP id 1

[ 1847.387404] Qman ErrInt: ecir.fqid 0xa0a

[ 1848.382325] Qman ErrInt: Invalid Enqueue State

[ 1848.385458] Qman ErrInt: DCP id 1

[ 1848.387458] Qman ErrInt: ecir.fqid 0xa0a

[ 1849.382280] Qman ErrInt: Invalid Enqueue State

[ 1849.385413] Qman ErrInt: DCP id 1

[ 1849.387413] Qman ErrInt: ecir.fqid 0xa0a

[ 1850.382251] Qman ErrInt: Invalid Enqueue State

[ 1850.385384] Qman ErrInt: DCP id 1

[ 1850.387384] Qman ErrInt: ecir.fqid 0xa0a

[ 1851.180110] fsl_dpa ethernet.18 fm2-gb0: Err FD status = 0x00004000

[ 1851.383162] fsl_dpa ethernet.18 fm2-gb0: Err FD status = 0x00004000

[ 1852.180167] fsl_dpa ethernet.18 fm2-gb0: Err FD status = 0x00004000

[ 1852.385166] fsl_dpa ethernet.18 fm2-gb0: Err FD status = 0x00004000

[ 1853.180226] fsl_dpa ethernet.18 fm2-gb0: Err FD status = 0x00004000

[ 1853.387196] fsl_dpa ethernet.18 fm2-gb0: Err FD status = 0x00004000

[ 1873.785371] Qman ErrInt: Invalid Enqueue State

[ 1873.788504] Qman ErrInt: DCP id 1

[ 1873.790504] Qman ErrInt: ecir.fqid 0xa1f

[ 1874.933720] Qman ErrInt: Invalid Enqueue State

[ 1874.936853] Qman ErrInt: DCP id 1

[ 1874.938853] Qman ErrInt: ecir.fqid 0xa1f

[ 1874.988160] Qman ErrInt: Invalid Enqueue State

[ 1874.991289] Qman ErrInt: DCP id 1

[ 1874.993289] Qman ErrInt: ecir.fqid 0xa1f

[ 1875.683596] Qman ErrInt: Invalid Enqueue State

[ 1875.686728] Qman ErrInt: DCP id 1

[ 1875.688727] Qman ErrInt: ecir.fqid 0xa1f

[ 1875.737567] Qman ErrInt: Invalid Enqueue State

[ 1875.740696] Qman ErrInt: DCP id 1

[ 1875.742696] Qman ErrInt: ecir.fqid 0xa1f

[ 1876.433597] Qman ErrInt: Invalid Enqueue State

[ 1876.436729] Qman ErrInt: DCP id 1

[ 1876.438729] Qman ErrInt: ecir.fqid 0xa1f

[ 1876.487691] Qman ErrInt: Invalid Enqueue State

[ 1876.490820] Qman ErrInt: DCP id 1

[ 1876.492820] Qman ErrInt: ecir.fqid 0xa1f

[ 1933.785859] Qman ErrInt: Invalid Enqueue State

[ 1933.788992] Qman ErrInt: DCP id 1

[ 1933.790992] Qman ErrInt: ecir.fqid 0xa1f

[ 1949.736065] Qman ErrInt: Invalid Enqueue State

[ 1949.739198] Qman ErrInt: DCP id 1

[ 1949.741198] Qman ErrInt: ecir.fqid 0xa1f

[ 1950.485989] Qman ErrInt: Invalid Enqueue State

[ 1950.489123] Qman ErrInt: DCP id 1

[ 1950.491123] Qman ErrInt: ecir.fqid 0xa1f

[ 1951.235940] Qman ErrInt: Invalid Enqueue State

[ 1951.239073] Qman ErrInt: DCP id 1

[ 1951.241073] Qman ErrInt: ecir.fqid 0xa1f

[ 1955.997457] Qman ErrInt: Invalid Enqueue State

[ 1956.000590] Qman ErrInt: DCP id 1

[ 1956.002590] Qman ErrInt: ecir.fqid 0xa1f

[ 1956.747361] Qman ErrInt: Invalid Enqueue State

[ 1956.750494] Qman ErrInt: DCP id 1

[ 1956.752494] Qman ErrInt: ecir.fqid 0xa1f

[ 1957.497307] Qman ErrInt: Invalid Enqueue State

[ 1957.500441] Qman ErrInt: DCP id 1

[ 1957.502441] Qman ErrInt: ecir.fqid 0xa1f

[ 2182.912437] Qman ErrInt: Invalid Enqueue State

[ 2182.915570] Qman ErrInt: DCP id 1

[ 2182.917570] Qman ErrInt: ecir.fqid 0xa1f

[ 2183.662633] Qman ErrInt: Invalid Enqueue State

[ 2183.665766] Qman ErrInt: DCP id 1

[ 2183.667766] Qman ErrInt: ecir.fqid 0xa1f

[ 2184.412574] Qman ErrInt: Invalid Enqueue State

[ 2184.415707] Qman ErrInt: DCP id 1

[ 2184.417707] Qman ErrInt: ecir.fqid 0xa1f

[ 2186.530422] Qman ErrInt: Invalid Enqueue State

[ 2186.533555] Qman ErrInt: DCP id 1

[ 2186.535555] Qman ErrInt: ecir.fqid 0xa1f

[ 2187.279673] Qman ErrInt: Invalid Enqueue State

[ 2187.282806] Qman ErrInt: DCP id 1

[ 2187.284806] Qman ErrInt: ecir.fqid 0xa1f

[ 2188.029775] Qman ErrInt: Invalid Enqueue State

[ 2188.032904] Qman ErrInt: DCP id 1

[ 2188.034904] Qman ErrInt: ecir.fqid 0xa1f

[ 2189.342150] Qman ErrInt: Invalid Enqueue State

[ 2189.345283] Qman ErrInt: DCP id 1

[ 2189.347283] Qman ErrInt: ecir.fqid 0xa1f

[ 2190.091818] Qman ErrInt: Invalid Enqueue State

[ 2190.094948] Qman ErrInt: DCP id 1

[ 2190.096947] Qman ErrInt: ecir.fqid 0xa1f

[ 2190.841927] Qman ErrInt: Invalid Enqueue State

[ 2190.845059] Qman ErrInt: DCP id 1

[ 2190.847058] Qman ErrInt: ecir.fqid 0xa1f

[ 2194.024453] Qman ErrInt: Invalid Enqueue State

[ 2194.027586] Qman ErrInt: DCP id 1

[ 2194.029586] Qman ErrInt: ecir.fqid 0xa1f

[ 2194.774137] Qman ErrInt: Invalid Enqueue State

[ 2194.777270] Qman ErrInt: DCP id 1

[ 2194.779270] Qman ErrInt: ecir.fqid 0xa1f

[ 2195.524276] Qman ErrInt: Invalid Enqueue State

[ 2195.527409] Qman ErrInt: DCP id 1

[ 2195.529409] Qman ErrInt: ecir.fqid 0xa1f

[ 2211.378941] Qman ErrInt: Invalid Enqueue State

[ 2211.382074] Qman ErrInt: DCP id 1

[ 2211.384073] Qman ErrInt: ecir.fqid 0xa1f

[ 2212.128110] Qman ErrInt: Invalid Enqueue State

[ 2212.131243] Qman ErrInt: DCP id 1

[ 2212.133242] Qman ErrInt: ecir.fqid 0xa1f

[ 2212.878219] Qman ErrInt: Invalid Enqueue State

[ 2212.881350] Qman ErrInt: DCP id 1

[ 2212.883350] Qman ErrInt: ecir.fqid 0xa1f

 

Also attaching the u-boot log for your reference.

 

Thanks,

Sharath Chandra

Original Attachment has been moved to: UBoot-Log.txt.zip

ラベル(1)
0 件の賞賛
2 返答(返信)

452件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Sharath Chandra,

You are using usdpaa dts and all the ethernet ports have been assigned to USDPAA, if you want to use the specific interface in Linux, please delete the related ethernet port definition in  "fsl,dpaa" part of p4080ds-usdpaa.dts.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

452件の閲覧回数
sharathchandra
Contributor II

Hi Yiping,

Will try that.

Thanks,

Sharath Chandra

0 件の賞賛