Where can I get the corresponding MAC address during setting up of environment

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where can I get the corresponding MAC address during setting up of environment

476件の閲覧回数
peterzheng
Contributor II

Hi,

I was trying to follow the document to set up the environment in p4080ds.

http://cache.freescale.com/files/soft_dev_tools/doc/support_info/QorIQ-SDK-1.6-IC-RevB.pdf

When I reach the 4.2.1.3 Configuring U-Boot network Parameters, it requires me to set the MAC addresses. May I ask where can I find the correct MAC addresses?

Thanks & Regards,

Peter

ラベル(1)
タグ(3)
0 件の賞賛
1 返信

270件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hello Peter Zheng,

In MAC address, the first 24 bits are OUI(Organizationally Unique Identifier), which is from IEEE for each factory. The rest 24 bits are set by factory.

Here 00-04-9F is for Freescale and 00-E0-0C is for MOTO. For test purpose, I think you can set MAC yourself, just make it differs from other MAC in your locally administered address space.

00-E0-0C      (hex)          MOTOROLA

00E00C        (base 16)    MOTOROLA

                                      5401 N. BEACH ST. S243

                                      FT. WORTH TX 76137

                                      UNITED STATES

00-04-9F      (hex)          Freescale Semiconductor

00049F        (base 16)    Freescale Semiconductor

                                    7700 West Parmer Lane

                                    MD PL59

                                    Austin TX 78729

                                    UNITED STATES


Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛