Where can I find the Linux application examples for p4080ds

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where can I find the Linux application examples for p4080ds

678 Views
gaolixing
Contributor I

hello,i am new to p4080ds,now i can compile a "hello world" program for p4080ds,and it run successfully on p4080ds,but p4080 is a complex soc,Where can I find the Linux application examples for p4080ds,for example,linux application example for DPAA,PCIE,and so on

Labels (1)
0 Kudos
2 Replies

618 Views
Pavel
NXP Employee
NXP Employee

See the Sections 7.4, 7.11 in SDK 1.9 documentation:

https://freescaleesd.flexnetoperations.com/337170/647/10318647/QORIQ-SDK-1-9_RN.pdf?ftpRequestID=776...

 

These documentation contains information about using DPAA, PCI and other interfaces for SDK 1.9 Linux BSP.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

619 Views
gaolixing
Contributor I

and where can i find the manual for the specific linux api for p4080 soc in sdk2.0 version

0 Kudos