SerDes 0x02 for p2041rdb available?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SerDes 0x02 for p2041rdb available?

Jump to solution
1,449 Views
norabjorklund
Contributor II


Hi,

I need to boot p2041rdb with SRIO configured, the user-guide claims I should load an RCW with serdes protocol 0x02. Is there a RCW available with the 0x02 protocol that I can use?

Best Regards,
Nora

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
1,061 Views
alexander_yakov
NXP Employee
NXP Employee

Sorry, we do not offer ready-to-use RCW values for any possible customer configurations. We expect our customers will create their own RCWs for their purposes.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
6 Replies
1,061 Views
norabjorklund
Contributor II

Okay, thanks for the quick reply.

I found this guide from sdk 1.9 documentation that I followed Submit Form​: which for the SRA application on p2041rdb states that I should use the following RCW:

00000000: AA55 AA55 010E 0100 1260 0000 0000 0000

00000010: 241C 0000 0000 0000 0899 30C0 C7C0 2000

00000020: FE80 0000 4000 0000 0000 0000 0000 0000

00000030: 0000 0000 D003 0F07 0000 0000 0000 0000

00000040: 0000 0000 0000 0000 0813 8040 57B0 F7D9

I followed the steps in the SRA guide, but I am getting this text in uboot (see bold text):

Reset Configuration Word (RCW):

       00000000: 12600000 00000000 241c0000 00000000

       00000010: 089930c0 c7c02000 fe800000 40000000

       00000020: 00000000 00000000 00000000 d0030f07

       00000030: 00000000 00000000 00000000 00000000

Board: P2041RDB, CPLD version: 4.1 vBank: 1

SERDES Reference Clocks: Bank1=100Mhz Bank2=125Mhz

I2C:   ready

SPI:   ready

DRAM:  Initializing....using SPD

Detected UDIMM CT51264BF1339.C16F

2 GiB left unmapped

Testing 0x00000000 - 0x7fffffff

Testing 0x80000000 - 0xffffffff

Remap DDR 2 GiB left unmapped

4 GiB (DDR3, 64-bit, CL=9, ECC off)

       DDR Chip-Select Interleaving Mode: CS0+CS1

POST memory PASSED

Flash: 128 MiB

L2:    128 KiB enabled

Corenet Platform Cache: 1 MiB enabled

SERDES: bank 3 disabled

SRIO1: enabled but port error

SRIO2: disabled

NAND:  512 MiB

MMC:   FSL_SDHC: 0

EEPROM: Invalid ID (ff ff ff ff)

PCIe1: Root Complex, no link, regs @ 0xfe200000

What can cause this port error?

0 Kudos
Reply
1,061 Views
genggeng
Contributor II

hi, i also meet this problem, have you resolved it ? and how to ?

thanks.

0 Kudos
Reply
1,061 Views
norabjorklund
Contributor II

Yes I got SRIO working on p2041rdb by following the guide for the SRA app in the qoriq sdk. I needed to set the boards cpld's multiplexers in u-boot and also set usdpaa_mem=64M. 

The cpld setting in u-boot was:

/* Especially the first one is important, there are descriptions in the datasheet of what values gives what setting. */
cpld_cmd lane_mux 6 0 

cpld_cmd lane_mux a 0

cpld_cmd lane_mux c 0

cpld_cmd lane_mux d 0

cpld reset altbank  /* I had a broken altbank so I did not use this command from what I remember */

Also good to keep in mind is that the usdpaa_mem boot variable cannot be larger than 64M (ie. usdpaa_mem=64M), else I couldn't use the usdpaa features...

0 Kudos
Reply
1,061 Views
genggeng
Contributor II

thanks for your quick reply.

when i configure serdes as 0x11, the two srio ports configured as two 2x,

when booting show this err at u-boot

********************************

SERDES: bank 3 disabled

SRIO1: enabled but port error

SRIO2: enabled but port error

NAND:  512 MiB

***************************************

i use the u-boot 2016.1 version released by QorIQ Linux SDK 2.0,

it seems an fiexed err at function 

srio_erratum_a004034() @ u-boot-2016.01-r0\arch\powerpc\cpu\mpc8xxx\srio.c

but it seems does not work.

In linux, i use usdpaa for srio and rman test, is there a good example to test doorbell?

in usdpaa-app i only found doorbell example tested with rmu, but not rman.

thanks, hope for your reply.

0 Kudos
Reply
1,062 Views
alexander_yakov
NXP Employee
NXP Employee

Sorry, we do not offer ready-to-use RCW values for any possible customer configurations. We expect our customers will create their own RCWs for their purposes.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,061 Views
norabjorklund
Contributor II

(Sorry for posting double but since it didn't seem like it was visible earlier)

I found this guide from sdk 1.9 documentation that I followed Submit Form: which for the SRA application on p2041rdb states that I should use the following RCW:

00000000: AA55 AA55 010E 0100 1260 0000 0000 0000

00000010: 241C 0000 0000 0000 0899 30C0 C7C0 2000

00000020: FE80 0000 4000 0000 0000 0000 0000 0000

00000030: 0000 0000 D003 0F07 0000 0000 0000 0000

00000040: 0000 0000 0000 0000 0813 8040 57B0 F7D9

I followed the steps in the SRA guide, but I am getting this text in uboot (see bold text below):

Reset Configuration Word (RCW):

       00000000: 12600000 00000000 241c0000 00000000

       00000010: 089930c0 c7c02000 fe800000 40000000

       00000020: 00000000 00000000 00000000 d0030f07

       00000030: 00000000 00000000 00000000 00000000

Board: P2041RDB, CPLD version: 4.1 vBank: 1

SERDES Reference Clocks: Bank1=100Mhz Bank2=125Mhz

I2C:   ready

SPI:   ready

DRAM:  Initializing....using SPD

Detected UDIMM CT51264BF1339.C16F

2 GiB left unmapped

Testing 0x00000000 - 0x7fffffff

Testing 0x80000000 - 0xffffffff

Remap DDR 2 GiB left unmapped

4 GiB (DDR3, 64-bit, CL=9, ECC off)

       DDR Chip-Select Interleaving Mode: CS0+CS1

POST memory PASSED

Flash: 128 MiB

L2:    128 KiB enabled

Corenet Platform Cache: 1 MiB enabled

SERDES: bank 3 disabled

SRIO1: enabled but port error

SRIO2: disabled

NAND:  512 MiB

MMC:   FSL_SDHC: 0

EEPROM: Invalid ID (ff ff ff ff)

PCIe1: Root Complex, no link, regs @ 0xfe200000

What can cause this port error?

0 Kudos
Reply