SEC 4.4 for P1010.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SEC 4.4 for P1010.

652件の閲覧回数
tsybezoff
Contributor II

When can i find an example of code with job decriptor MATH functions???

ラベル(1)
タグ(1)
0 件の賞賛
3 返答(返信)

480件の閲覧回数
bpe
NXP Employee
NXP Employee


Unpack QorIQ SDK package called "flib" and grep files in  tests/
directory  for "math". There are many descriptors that use
SEC math operations.

More information on QorIQ SDK:

Linux® SDK for QorIQ Processors|NXP 


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

480件の閲覧回数
tsybezoff
Contributor II

I downloaded 3 ISO-file and can't find examples((

0 件の賞賛

480件の閲覧回数
tsybezoff
Contributor II

QorIQ Linux SDK v2.0 SOURCE.iso ???

0 件の賞賛