P5020 PCIe lane reversal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P5020 PCIe lane reversal

1,389 Views
kyleb
Contributor I

Hello, I am using a P5020 where the PCIe controller 1 is configured as a x4 and the PCIe controller 2 is configured as a x1. The PCIe x4 enumerates but the x1 does not. One possible reason is due to the x1 being connected to Lane H on the P5020 (signal names SD_RX07, SD_TX07, and their complements) rather than the perhaps preferred Lane E. NXP has indicated that the PCIe controller does have the ability to perform a lane reversal, but I do not see anything that indicates whether this is an automatic process or something that must be commanded via a register?

Thanks in advance!

Labels (1)
0 Kudos
3 Replies

786 Views
ufedor
NXP Employee
NXP Employee

PEX2 is an x4 controller. Therefore, it should work with lane reversal with Lane 0 routed to Bank 1 Lane H.

0 Kudos

786 Views
kyleb
Contributor I

Thank you for the reply. Is lane reversal an automatic process or must the P5020 be directed (through a register write or similar) to do the lane reversal? I have not found much documentation on the subject. Thanks

0 Kudos

786 Views
ufedor
NXP Employee
NXP Employee

Yes, lane reversal is automatic.

0 Kudos