dear experts!
I want to add srio to linux kernel for my customized P2020 board!
I am using yocto 1.7, my modification of dtb are as follows:
a)in p2020rdb-pc.dtsi, i added rmu:
rmu: rmu@d3000 {
#address-cells = <1>;
#size-cells = <1>;
compatible = "fsl,srio-rmu";
reg = <0xd3000 0x500>;
ranges = <0x0 0xd3000 0x500>;
message-unit@0 {
compatible = "fsl,srio-msg-unit";
reg = <0x0 0x100>;
interrupts = <
60 2 0 0 /* msg1_tx_irq */
61 2 0 0>;/* msg1_rx_irq */
};
message-unit@100 {
compatible = "fsl,srio-msg-unit";
reg = <0x100 0x100>;
interrupts = <
62 2 0 0 /* msg2_tx_irq */
63 2 0 0>;/* msg2_rx_irq */
};
doorbell-unit@400 {
compatible = "fsl,srio-dbell-unit";
reg = <0x400 0x80>;
interrupts = <
56 2 0 0 /* bell_outb_irq */
57 2 0 0>;/* bell_inb_irq */
};
port-write-unit@4e0 {
compatible = "fsl,srio-port-write-unit";
reg = <0x4e0 0x20>;
interrupts = <16 2 1 11>;
};
};
b) in p2020rdb-pc_32b.dts
1.i added:
rio: rapidio@ffe0c0000 {
reg = <0xf 0xfe0c0000 0 0x11000>;
port1 {
ranges = <0 0 0xc 0x20000000 0 0x10000000>;
};
};
2. comment out pci0,pci1,and pci2.
c)in p2020si-post.dtsi
1. added:
&rio {
compatible = "fsl,srio";
interrupts = <48 2 0 0>;
#address-cells = <2>;
#size-cells = <2>;
fsl,srio-rmu-handle = <&rmu>;
/*sleep = <&pmc 0x00080000>;*/
ranges;
port1 {
#address-cells = <2>;
#size-cells = <2>;
cell-index = <1>;
};
because pmc is undefined ,so i comment out this line "sleep = <&pmc 0x00080000>;"
i guess linux kernel stoped at srio driver init, the console print are as follows:
fsl-l2ctlr ffe20000.l2-cache-controller: Entire L2 as cache, provide valid sram address and size
fsl-l2ctlr: probe of ffe20000.l2-cache-controller failed with error -22
Setting up RapidIO peer-to-peer network /rapidio@ffe0c0000
fsl-of-rio ffe0c0000.rapidio: Of-device full name /rapidio@ffe0c0000
fsl-of-rio ffe0c0000.rapidio: Regs: [mem 0xffe0c0000-0xffe0d0fff]
fsl-of-rio ffe0c0000.rapidio: bellirq: 57
fsl-of-rio ffe0c0000.rapidio: pwirq: 16
fsl-of-rio ffe0c0000.rapidio: /rapidio@ffe0c0000/port1: LAW start 0x0000000c20000000, size 0x0000000010000000.
解決済! 解決策の投稿を見る。
Have figured it out!
1.i added:
rio: rapidio@ffe0c0000 {
reg = <0xf 0xfe0c0000 0 0x11000>;
the register is wrong ,it should be reg = <0x0 0xfe0c0000 0 0x11000>;
now kernel boots ok! the print are as follows:
fsl-l2ctlr: probe of ffe20000.l2-cache-controller failed with error -22
Setting up RapidIO peer-to-peer network /rapidio@0xffec0000
fsl-of-rio ffec0000.rapidio: Of-device full name /rapidio@0xffec0000
fsl-of-rio ffec0000.rapidio: Regs: [mem 0xffec0000-0xffed0fff]
fsl-of-rio ffec0000.rapidio: bellirq: 50
fsl-of-rio ffec0000.rapidio: pwirq: 48
fsl-of-rio ffec0000.rapidio: /rapidio@0xffec0000/port2: LAW start 0x0000000c20000000, size 0x0000000010000000.
fsl-of-rio ffec0000.rapidio: RapidIO PHY type: Serial
fsl-of-rio ffec0000.rapidio: Hardware port width: 4
fsl-of-rio ffec0000.rapidio: Training connection status: Four-lane
fsl-of-rio ffec0000.rapidio: RapidIO Common Transport System size: 256
/soc@ffe00000/rmu@d3000/message-unit@100: txirq: 55, rxirq 56
anybody knows how to use srio to write another device? how to develop the application?
Use the following link:
Have a great day,
Pavel Chubakov
Thank you Pavel Chubakov,I have a question about how to use rapidio demo on p2020.did there any demo about how to use rapidio on p2020 which use linux kernel 3.12.And I use Yocto SDK 1.8 。I found SDK only have a rionet demo and i want a demo which like rmu in usdpaa-apps? Did there any? Sorry for my little English!
Have figured it out!
1.i added:
rio: rapidio@ffe0c0000 {
reg = <0xf 0xfe0c0000 0 0x11000>;
the register is wrong ,it should be reg = <0x0 0xfe0c0000 0 0x11000>;
now kernel boots ok! the print are as follows:
fsl-l2ctlr: probe of ffe20000.l2-cache-controller failed with error -22
Setting up RapidIO peer-to-peer network /rapidio@0xffec0000
fsl-of-rio ffec0000.rapidio: Of-device full name /rapidio@0xffec0000
fsl-of-rio ffec0000.rapidio: Regs: [mem 0xffec0000-0xffed0fff]
fsl-of-rio ffec0000.rapidio: bellirq: 50
fsl-of-rio ffec0000.rapidio: pwirq: 48
fsl-of-rio ffec0000.rapidio: /rapidio@0xffec0000/port2: LAW start 0x0000000c20000000, size 0x0000000010000000.
fsl-of-rio ffec0000.rapidio: RapidIO PHY type: Serial
fsl-of-rio ffec0000.rapidio: Hardware port width: 4
fsl-of-rio ffec0000.rapidio: Training connection status: Four-lane
fsl-of-rio ffec0000.rapidio: RapidIO Common Transport System size: 256
/soc@ffe00000/rmu@d3000/message-unit@100: txirq: 55, rxirq 56
anybody knows how to use srio to write another device? how to develop the application?
Look at the following page:
http://www.freescale.com/infocenter/index.jsp?topic=%2FQORIQSDK%2F2151439.html
excause me,The page have missing? can tell where i can find the lastest?