P1022 DDR3 Clk Range

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,077件の閲覧回数
nishad_kamdar
Contributor IV

I am using a Custom board with P1022 Processor on it.

I was going through the P1022DS reference manual which says that the DDR3 Clock is Asynchronous and is set at a frequency of 667MHz.

However, the Design Checklist of P1022 Processor (AN4343 Page 14) says that the maximum frequency for DDR3 Controller is 400MHz.

Could someone explain how will this work?

Is there something i am missing here ? 

ラベル(1)
タグ(2)
1 解決策
701件の閲覧回数
Bulat
NXP Employee
NXP Employee

The P1022DS reference manual refers to the data rate frequency (667MHz), this corresponds to the DDR clock frequency of 333.3 MHz.

The AN4343 explicitly says that the maximum frequency of 400MHz assumes MCK[0:5] clock outputs, this corresponds to the data rate of 800MHz. So there is no contradiction, P1022DS runs DDR3 interface at proper frequency, within specified frequency range.

元の投稿で解決策を見る

0 件の賞賛
3 返答(返信)
701件の閲覧回数
nishad_kamdar
Contributor IV

Ok

Now i get it.

Thanks for the reply.

0 件の賞賛
701件の閲覧回数
hermann_ruckerb
Contributor III

Hi,

This was a common mistake in the beginning of DDR Memory: Mixing MHz and Mb/s. Frequency need to be given in MHz and Datarate in Mb/s.  I'm a bit surprised to see such a mistake today...

Correct usage would be to give the Clock frequency in MHz, e. g. 400MHz.

The corresponding datarate for the Databus would be 800Mb/s. The maximum Frequency you could see on the Databus is still 400MHz for a clock like 10101 pattern.

The CA bus is still Single Datarate, so for a 400MHz CLK we do have 400Mb/s on the CA bus. The max. Frequency you can see on the CA signal is 200MHz for a 10101 like pattern.

Hermann

702件の閲覧回数
Bulat
NXP Employee
NXP Employee

The P1022DS reference manual refers to the data rate frequency (667MHz), this corresponds to the DDR clock frequency of 333.3 MHz.

The AN4343 explicitly says that the maximum frequency of 400MHz assumes MCK[0:5] clock outputs, this corresponds to the data rate of 800MHz. So there is no contradiction, P1022DS runs DDR3 interface at proper frequency, within specified frequency range.

0 件の賞賛