Hello,
I would like to configure the field FTIM1 and FTIM2.
I am using a driver in the attachment file, that it was configurated the access to the memory with the .dtb file generating the lbc_teste.
I have the configurations to the LocalBus showed in the file xilinx.c, but only the register TACO change like I want.
The others registers like the TRAD_NOR, TCS, TCH, TWPH and TWP do not change the width in the oscilloscope.
I would like some help to resolve this problem, because I am accessing a device slower than the P1010.
Thanks,
Fábio Walter.
Original Attachment has been moved to: xilinx.c.zip
Please try to configure FTIMn in u-boot include/configs/P1010RDB.h.
/* NOR Flash Timing Params */
#define CONFIG_SYS_NOR_FTIM0>---FTIM0_NOR_TACSE(0x4) | \
>--->--->--->---FTIM0_NOR_TEADC(0x5) | \
>--->--->--->---FTIM0_NOR_TEAHC(0x5)
#define CONFIG_SYS_NOR_FTIM1>---FTIM1_NOR_TACO(0x1e) | \
>--->--->--->---FTIM1_NOR_TRAD_NOR(0x0f)
#define CONFIG_SYS_NOR_FTIM2>---FTIM2_NOR_TCS(0x4) | \
>--->--->--->---FTIM2_NOR_TCH(0x4) | \
>--->--->--->---FTIM2_NOR_TWP(0x1c)
#define CONFIG_SYS_NOR_FTIM3>---0x0