I want access CPLD by use IFC of P1010 chip. so I config it
by reference the configuration of NorFlash ,but it don't work.
So , I want get the answer , how can I config the P1010 chip for
access CPLD. could you send out an example of the IFC config.
My configuration sequence is :
Step 1, Set TLB :
Set MAS0 , MAS1, MAS2,MAS3 registers value.
Step2, Config IFC interface :
Set IFC_CSPR3, IFC_CSOR3, IFC_FTIM0_CS3
Set IFC_FTIM2_CS3,IFC_FTIM2_CS3,IFC_FTIM3_CS3
Step3, Set LAW access:
Set LAWBAR3, LAWAR3
Step4, GPIO PUMX:
Set GUTS_PMUXCR1 .
(I have try to set and reset LCLK bits in GUTS_PMUXCR1).
The attachment is configration code in ASM .
Regards,
XieJianwei
Original Attachment has been moved to: romInit.s.zip
已解决! 转到解答。
Hi,
Please find attached the initialization file used by us in CodeWarrior for P1010RDB (this contains the full initialization for DDR, NOR and CPLD - you can take a look only at the CPLD side).
Please note that:
- we're moving the CCSRBAR at 0xE000_0000 (you'll need to update the code according with your ccsrbar value)
- the code is for EWL compiler (you'll need to update the asm instructions to your compiler)
- the CPLD initialization flow is the next one:
- TLB init
- LAW init
- IFC controller init
- CPLD regs init
Regards,
Marius
FAE say , the configuration is correct, The configuration is same to uboot. there may be have something wrong with multiplexing on the P1010RDB .
so , we will try it on our designed board which have no multiplexing !
I have use this config in our board . Now I can read and write the FPGA . the config is correct. but the CPLD is still can't read and write.
the difference between FPGA and CPLD only 16-bit data and 8-bit data width wide differences
Hi,
Please find attached the initialization file used by us in CodeWarrior for P1010RDB (this contains the full initialization for DDR, NOR and CPLD - you can take a look only at the CPLD side).
Please note that:
- we're moving the CCSRBAR at 0xE000_0000 (you'll need to update the code according with your ccsrbar value)
- the code is for EWL compiler (you'll need to update the asm instructions to your compiler)
- the CPLD initialization flow is the next one:
- TLB init
- LAW init
- IFC controller init
- CPLD regs init
Regards,
Marius
Marius,
thank you, it's a useful reply.
I tried to use same configuration with the P1010RDB_init.c defined ,but i still read oxff from CPLD in p1010rdb borad.
The CPLD run the default program from Freescale.
I use Oscilloscope to Monitor IFC_CS3_N, the IFC_CS3_N is always at high voltage. why?
Regards,
Jianwei
Hi Jianwei,
I just found an errata A-003549 about CS3 at P1010 RDB. You can read about it here [1].
Secondly, I observed that I can read the CPLD registers from u-boot without issues. The u-boot maps the CPLD starting from 0xffb00000 - if you want make a try. I will investigate if the u-boot is making any additional workarounds for accessing the CPLD registers and I'll let you know the results ASAP.
Regards,
Marius
[1] http://www.freescale.com/docs/pcn_attachments/15629_P1010CE_RevL.pdf
Hi Marius,
I use uboot to load vxworks running in ram, under vxworks it can read CPLD value correctly.
SO , I'm sure issue lies in the configuration file, but the config is seem same as uboot configuration.
I don't know how to check issues.
Regards,
Jianwei
Hi Marius,
under uboot, i read address 0xffb00000, this address value is 3.
It shows under uboot configuration ,the CPLD is working properly.
But under vxworks, i can't read correct value from CPLD.
then I check the config . It looks the same as the code you give me.
i have configed the pmuxcr1 LCLK to (11b). The cs3 seems no action.
The read out register is :
->
Break at 0x0010f38c: ifcTst +0x14 Task: 0x49b1be0 (tIfcTst)
IFC_REV Address =ffe1e000, value = 1000000
IFC_CSPR0 Address =ffe1e010, value = 105
IFC_CSPR1 Address =ffe1e01c, value = 0
IFC_CSPR2 Address =ffe1e028, value = 0
IFC_CSPR3 Address =ffe1e034, value = ffb00085
IFC_AMASK0 Address =ffe1e0a0, value = 0
IFC_AMASK1 Address =ffe1e0ac, value = 0
IFC_AMASK2 Address =ffe1e0b8, value = 0
IFC_AMASK3 Address =ffe1e0c4, value = ffff0000
IFC_CSOR0 Address =ffe1e130, value = e00c
IFC_CSOR1 Address =ffe1e13c, value = c
IFC_CSOR2 Address =ffe1e148, value = c
IFC_CSOR3 Address =ffe1e154, value = 0
IFC_FTIM0_CS0 Address =ffe1e1c0, value = 40050005
IFC_FTIM1_CS0 Address =ffe1e1c4, value = 1e000f00
IFC_FTIM2_CS0 Address =ffe1e1c8, value = 410001c
IFC_FTIM3_CS0 Address =ffe1e1cc, value = 0
IFC_FTIM0_CS1 Address =ffe1e1f0, value = 0
IFC_FTIM1_CS1 Address =ffe1e1f4, value = 0
IFC_FTIM2_CS1 Address =ffe1e1f8, value = 0
IFC_FTIM3_CS1 Address =ffe1e1fc, value = 0
IFC_FTIM0_CS2 Address =ffe1e220, value = 0
IFC_FTIM1_CS2 Address =ffe1e224, value = 0
IFC_FTIM2_CS2 Address =ffe1e228, value = 0
IFC_FTIM3_CS2 Address =ffe1e22c, value = 0
IFC_FTIM0_CS3 Address =ffe1e250, value = e00e000e
IFC_FTIM1_CS3 Address =ffe1e254, value = e001f00
IFC_FTIM2_CS3 Address =ffe1e258, value = e00001f
IFC_FTIM3_CS3 Address =ffe1e25c, value = 0
IFC_RB_STAT Address =ffe1e400, value = f0000000
IFC_GCR Address =ffe1e40c, value = 2800
IFC_EVTER_STAT Address =ffe1e418, value = 0
IFC_GPCM_EVTER_STAT Address =ffe1f800, value = 0
IFC_GPCM_ERATTRO Address =ffe1f824, value = 0
IFC_GPCM_ERATTR1 Address =ffe1f828, value = 0
IFC_GPCM_ERATTR2 Address =ffe1f82c, value = 0
-> d 0xffe1e44c,1,4
NOTE: memory values are displayed in hexadecimal.
0xffe1e440: 03008000 * *
value = 0 = 0x0
-> d 0xffe1e40c,1,4
NOTE: memory values are displayed in hexadecimal.
0xffe1e400: 00002800 * ( *
value = 0 = 0x0
-> d 0xffee0060,1,4
NOTE: memory values are displayed in hexadecimal.
0xffee0060: 000000c0 *................*
value = 0 = 0x0
-> d 0xffb00000,1,1
NOTE: memory values are displayed in hexadecimal.
0xffb00000: ff *................*
value = 0 = 0x0
->
Regards,
Jianwei