Is the P1022 processor compatible with the Nand Flash which's page size is over 4KB ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is the P1022 processor compatible with the Nand Flash which's page size is over 4KB ?

566 次查看
chengliu
Contributor I

I see in the p1022rm datasheet that the p1022 is only compatible with small (512 + 16 bytes) and large (2048 + 64 bytes) page parallel NAND Flash. Thanks!

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

500 次查看
alexander_yakov
NXP Employee
NXP Employee

No, 4K page size is not supported.

500 次查看
chengliu
Contributor I

Thank you very much!

0 项奖励
回复