Installation of QorIq SDK on Ubuntu 12.04

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Installation of QorIq SDK on Ubuntu 12.04

4,875件の閲覧回数
hitusharma
Contributor II

While installing I am getting this error:

root@embedded-HP-Z210-SFF-Workstation:~/QorIQ-SDK-V1.6-20140619-yocto# ./fsl-setup-poky – m p1020rdb

bash: ./fsl-setup-poky: Permission denied

kindly resolve

ラベル(1)
0 件の賞賛
返信
23 返答(返信)

2,552件の閲覧回数
hitusharma
Contributor II

Hi Yiping

How to access the toolchan available in ver1.6.?

wrt the link shared in the last response, should have the access to sysroots, shall i Have to install it!!!

regards

Hitu

0 件の賞賛
返信

2,552件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Hitu,

The pre_built Toolchain is provided in the images ISO, you could install it and source the environment script. This toolchain is standalone, if you need assistance to use it, you could create a new thread about this topic.

You also could use the Toolchain in provide in SDK Yocto build environment.

The Toolchin is in build_<platform>_release/tmp/sysroots/x86_64-linux/usr/bin/<processor>-fsl-linux/


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,553件の閲覧回数
hitusharma
Contributor II

HI Yiping

Thanks I am able to run bitbake netcf -c configure -f" successfully

Since I have install the Build environment for SDK and I a installing this on Ubuntu 12.04 and not on the virtual machine, do I need to get into UBoot and Linux kernal configuration as mentioned in the SDL document or I can directly install the tool can and can write a simple application in C??

regards

Hitu

0 件の賞賛
返信

2,552件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hi Hitu,

The SDK 1.6 images ISO has already  provided prebuilt Toolchain, you could use it to build your own application code? Please refer to Re: SDK cross-toolchain build error.

Why do you want to modify Kernel and u-boot? If you use the Freescale demo board, no need to modify them.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,553件の閲覧回数
hitusharma
Contributor II

Hi Yiping

while I am trying to clean the bitbake

its telling me that bitbake is not installed.nd install in using apt-get install bitbake.

embedded@embedded-HP-Z210-SFF-Workstation:~/QorIQ-SDK-V1.6-20140619-yocto/build_p2020rdb_release$ bitbake netcf -c clean

The program 'bitbake' is currently not installed.  You can install it by typing:

sudo apt-get install bitbake

I tried doing that but unable to install because I am getting error repeatedly.

Connection failed [IP: 91.189.88.149 80]

regds

Hitu

0 件の賞賛
返信

2,553件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Hitu,

Every time when you login the build server again.

Please run the command under the folder ~/QorIQ-SDK-V1.6-20140619-yocto/.

source ./fsl-setup-poky -m p2020rdb

or

In the folder ~/QorIQ-SDK-V1.6-20140619-yocto/build_p2020rdb_release.

execute "source SOURCE_THIS".


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,553件の閲覧回数
hitusharma
Contributor II

Hi Yiping

I tried installing installing  bitbake following is the installation steps and its stuck at a certain point.

embedded@embedded-HP-Z210-SFF-Workstation:~/QorIQ-SDK-V1.6-20140619-yocto/build_p2020rdb_release$ bitbake fsl-image-full

Loading cache: 100% |###########################################| ETA:  00:00:00

Loaded 2204 entries from dependency cache.

NOTE: Resolving any missing task queue dependencies

Build Configuration:

BB_VERSION        = "1.22.0"

BUILD_SYS         = "i686-linux"

NATIVELSBSTRING   = "Ubuntu-12.04"

TARGET_SYS        = "powerpc-fsl-linux-gnuspe"

MACHINE           = "p2020rdb"

DISTRO            = "fsl-networking"

DISTRO_VERSION    = "1.6"

TUNE_FEATURES     = "m32 spe ppce500v2"

TARGET_FPU        = "ppc-efd"

meta             

meta-yocto       

meta-yocto-bsp    = "(nobranch):0d2ce44c2b0f8cc9699e30cca2c24655be89d58b"

meta-fsl-ppc      = "(nobranch):6cf59d9de63a9fc5f8942c0d10c622898f4315ce"

meta-fsl-ppc-toolchain = "(nobranch):a546e42f86e7d57de19e27907365d170b13fc18f"

meta-fsl-networking

meta-fsl-networking = "(nobranch):8dec9c690188cce5305ef5055f91e5cfa35c63f4"

meta-virtualization

meta-virtualization = "(nobranch):8044073f63a0d99541a43ac5f2f6d789f94c7c7c"

meta-oe          

meta-networking  

meta-webserver   

meta-ruby        

meta-filesystems  = "(nobranch):b86007f742a1b829ccc8d76e485bb3f789cefaa4"

meta-java         = "(nobranch):d01f7d39e513790ddce20e6724723722119a3700"

meta-openstack   

meta-openstack-compute-deploy

meta-openstack-controller-deploy

meta-openstack-qemu = "(nobranch):f627404399a134672e0b5e26a0d9b794a6f8adf4"

NOTE: Preparing runqueue

NOTE: Executing SetScene Tasks

NOTE: Executing RunQueue Tasks

ERROR: Function failed: do_configure (log file is located at /home/embedded/QorIQ-SDK-V1.6-20140619-yocto/build_p2020rdb_release/tmp/work/ppce500v2-fsl-linux-gnuspe/netcf/0.2.2+gitAUTOINC+2b0d9ca226-r1/temp/log.do_configure.3627)

ERROR: Logfile of failure stored in: /home/embedded/QorIQ-SDK-V1.6-20140619-yocto/build_p2020rdb_release/tmp/work/ppce500v2-fsl-linux-gnuspe/netcf/0.2.2+gitAUTOINC+2b0d9ca226-r1/temp/log.do_configure.3627

Log data follows:

| DEBUG: Executing python function sysroot_cleansstate

| DEBUG: Python function sysroot_cleansstate finished

| DEBUG: SITE files ['endian-big', 'bit-32', 'powerpc-common', 'common-linux', 'common-glibc', 'powerpc-linux', 'powerpc32-linux', 'powerpc-linux-gnuspe', 'common']

| DEBUG: Executing shell function autotools_preconfigure

| DEBUG: Shell function autotools_preconfigure finished

| DEBUG: Executing python function autotools_copy_aclocals

| DEBUG: Python function autotools_copy_aclocals finished

| DEBUG: Executing shell function do_configure

| ./bootstrap: Bootstrapping from checked-out netcf sources...

| ./bootstrap: consider installing git-merge-changelog from gnulib

| ./bootstrap: getting gnulib files...

| Submodule 'gnulib' () registered for path '.gnulib'

| fatal: Needed a single revision

| Unable to find current revision in submodule path '.gnulib'

| WARNING: exit code 1 from a shell command.

| ERROR: Function failed: do_configure (log file is located at /home/embedded/QorIQ-SDK-V1.6-20140619-yocto/build_p2020rdb_release/tmp/work/ppce500v2-fsl-linux-gnuspe/netcf/0.2.2+gitAUTOINC+2b0d9ca226-r1/temp/log.do_configure.3627)

ERROR: Task 3507 (/home/embedded/QorIQ-SDK-V1.6-20140619-yocto/meta-virtualization/recipes-networking/netcf/netcf_git.bb, do_configure) failed with exit code '1'

NOTE: Tasks Summary: Attempted 2139 tasks of which 2135 didn't need to be rerun and 1 failed.

Waiting for 0 running tasks to finish:

Summary: 1 task failed:

  /home/embedded/QorIQ-SDK-V1.6-20140619-yocto/meta-virtualization/recipes-networking/netcf/netcf_git.bb, do_configure

Summary: There was 1 ERROR message shown, returning a non-zero exit code.

embedded@embedded-HP-Z210-SFF-Workstation:~/QorIQ-SDK-V1.6-20140619-yocto/build_p2020rdb_release$ bitbake netcf -c clean

Loading cache: 100% |###########################################| ETA:  00:00:00

Loaded 2204 entries from dependency cache.

NOTE: Resolving any missing task queue dependencies

Build Configuration:

BB_VERSION        = "1.22.0"

BUILD_SYS         = "i686-linux"

NATIVELSBSTRING   = "Ubuntu-12.04"

TARGET_SYS        = "powerpc-fsl-linux-gnuspe"

MACHINE           = "p2020rdb"

DISTRO            = "fsl-networking"

DISTRO_VERSION    = "1.6"

TUNE_FEATURES     = "m32 spe ppce500v2"

TARGET_FPU        = "ppc-efd"

meta             

meta-yocto       

meta-yocto-bsp    = "(nobranch):0d2ce44c2b0f8cc9699e30cca2c24655be89d58b"

meta-fsl-ppc      = "(nobranch):6cf59d9de63a9fc5f8942c0d10c622898f4315ce"

meta-fsl-ppc-toolchain = "(nobranch):a546e42f86e7d57de19e27907365d170b13fc18f"

meta-fsl-networking

meta-fsl-networking = "(nobranch):8dec9c690188cce5305ef5055f91e5cfa35c63f4"

meta-virtualization

meta-virtualization = "(nobranch):8044073f63a0d99541a43ac5f2f6d789f94c7c7c"

meta-oe          

meta-networking  

meta-webserver   

meta-ruby        

meta-filesystems  = "(nobranch):b86007f742a1b829ccc8d76e485bb3f789cefaa4"

meta-java         = "(nobranch):d01f7d39e513790ddce20e6724723722119a3700"

meta-openstack   

meta-openstack-compute-deploy

meta-openstack-controller-deploy

meta-openstack-qemu = "(nobranch):f627404399a134672e0b5e26a0d9b794a6f8adf4"

NOTE: Preparing runqueue

NOTE: Executing RunQueue Tasks

NOTE: Tasks Summary: Attempted 1 tasks of which 0 didn't need to be rerun and all succeeded.

embedded@embedded-HP-Z210-SFF-Workstation:~/QorIQ-SDK-V1.6-20140619-yocto/build_p2020rdb_release$  bitbake netcf -c patch

Loading cache: 100% |###########################################| ETA:  00:00:00

Loaded 2204 entries from dependency cache.

NOTE: Resolving any missing task queue dependencies

Build Configuration:

BB_VERSION        = "1.22.0"

BUILD_SYS         = "i686-linux"

NATIVELSBSTRING   = "Ubuntu-12.04"

TARGET_SYS        = "powerpc-fsl-linux-gnuspe"

MACHINE           = "p2020rdb"

DISTRO            = "fsl-networking"

DISTRO_VERSION    = "1.6"

TUNE_FEATURES     = "m32 spe ppce500v2"

TARGET_FPU        = "ppc-efd"

meta             

meta-yocto       

meta-yocto-bsp    = "(nobranch):0d2ce44c2b0f8cc9699e30cca2c24655be89d58b"

meta-fsl-ppc      = "(nobranch):6cf59d9de63a9fc5f8942c0d10c622898f4315ce"

meta-fsl-ppc-toolchain = "(nobranch):a546e42f86e7d57de19e27907365d170b13fc18f"

meta-fsl-networking

meta-fsl-networking = "(nobranch):8dec9c690188cce5305ef5055f91e5cfa35c63f4"

meta-virtualization

meta-virtualization = "(nobranch):8044073f63a0d99541a43ac5f2f6d789f94c7c7c"

meta-oe          

meta-networking  

meta-webserver   

meta-ruby        

meta-filesystems  = "(nobranch):b86007f742a1b829ccc8d76e485bb3f789cefaa4"

meta-java         = "(nobranch):d01f7d39e513790ddce20e6724723722119a3700"

meta-openstack   

meta-openstack-compute-deploy

meta-openstack-controller-deploy

meta-openstack-qemu = "(nobranch):f627404399a134672e0b5e26a0d9b794a6f8adf4"

NOTE: Preparing runqueue

NOTE: Executing SetScene Tasks

NOTE: Executing RunQueue Tasks

NOTE: Tasks Summary: Attempted 10 tasks of which 7 didn't need to be rerun and all succeeded.

embedded@embedded-HP-Z210-SFF-Workstation:~/QorIQ-SDK-V1.6-20140619-yocto/build_p2020rdb_release$  bitbake netcf -c configure -f

Loading cache: 100% |###########################################| ETA:  00:00:00

Loaded 2204 entries from dependency cache.

NOTE: Resolving any missing task queue dependencies

Build Configuration:

BB_VERSION        = "1.22.0"

BUILD_SYS         = "i686-linux"

NATIVELSBSTRING   = "Ubuntu-12.04"

TARGET_SYS        = "powerpc-fsl-linux-gnuspe"

MACHINE           = "p2020rdb"

DISTRO            = "fsl-networking"

DISTRO_VERSION    = "1.6"

TUNE_FEATURES     = "m32 spe ppce500v2"

TARGET_FPU        = "ppc-efd"

meta             

meta-yocto       

meta-yocto-bsp    = "(nobranch):0d2ce44c2b0f8cc9699e30cca2c24655be89d58b"

meta-fsl-ppc      = "(nobranch):6cf59d9de63a9fc5f8942c0d10c622898f4315ce"

meta-fsl-ppc-toolchain = "(nobranch):a546e42f86e7d57de19e27907365d170b13fc18f"

meta-fsl-networking

meta-fsl-networking = "(nobranch):8dec9c690188cce5305ef5055f91e5cfa35c63f4"

meta-virtualization

meta-virtualization = "(nobranch):8044073f63a0d99541a43ac5f2f6d789f94c7c7c"

meta-oe          

meta-networking  

meta-webserver   

meta-ruby        

meta-filesystems  = "(nobranch):b86007f742a1b829ccc8d76e485bb3f789cefaa4"

meta-java         = "(nobranch):d01f7d39e513790ddce20e6724723722119a3700"

meta-openstack   

meta-openstack-compute-deploy

meta-openstack-controller-deploy

meta-openstack-qemu = "(nobranch):f627404399a134672e0b5e26a0d9b794a6f8adf4"

NOTE: Preparing runqueue

NOTE: Tainting hash to force rebuild of task /home/embedded/QorIQ-SDK-V1.6-20140619-yocto/meta-virtualization/recipes-networking/netcf/netcf_git.bb, do_configure

NOTE: Executing SetScene Tasks

NOTE: Executing RunQueue Tasks

Currently 1 running tasks (354 of 354):

0: netcf-0.2.2+gitAUTOINC+2b0d9ca226-r1 do_configure (pid 6589)

its not moving ahead,what should i conclude from this..

regds

HItu

0 件の賞賛
返信

2,553件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hi Hitu,

Please try to use the workaround step by step, which I provided at "


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,553件の閲覧回数
hitusharma
Contributor II

Hi Yiping

I have followed the steps which u shared on Sep 10 2014, here is the sequence:

Step 1:

In the folder ~/QorIQ-SDK-V1.6-20140619-yocto/build_p2020rdb_release.

execute "source SOURCE_THIS

".

Step 2:

embedded@embedded-HP-Z210-SFF-Workstation:~/QorIQ-SDK-V1.6-20140619-yocto/build_p2020rdb_release$ bitbake fsl-image-full

ERROR: Function failed: do_configure (log file is located at /home/embedded/QorIQ-SDK-V1.6-20140619-yocto/build_p2020rdb_release/tmp/work/ppce500v2-fsl-linux-gnuspe/netcf/0.2.2+gitAUTOINC+2b0d9ca226-r1/temp/log.do_configure.3627)

ERROR: Logfile of failure stored in: /home/embedded/QorIQ-SDK-V1.6-20140619-yocto/build_p2020rdb_release/tmp/work/ppce500v2-fsl-linux-gnuspe/netcf/0.2.2+gitAUTOINC+2b0d9ca226-r1/temp/log.do_configure.3627

Unable to find current revision in submodule path '.gnulib'

| WARNING: exit code 1 from a shell command.

| ERROR: Function failed: do_configure (log file is located at /home/embedded/QorIQ-SDK-V1.6-20140619-yocto/build_p2020rdb_release/tmp/work/ppce500v2-fsl-linux-gnuspe/netcf/0.2.2+gitAUTOINC+2b0d9ca226-r1/temp/log.do_configure.3627)

ERROR: Task 3507 (/home/embedded/QorIQ-SDK-V1.6-20140619-yocto/meta-virtualization/recipes-networking/netcf/netcf_git.bb, do_configure) failed with exit code '1'

NOTE: Tasks Summary: Attempted 2139 tasks of which 2135 didn't need to be rerun and 1 failed.

Waiting for 0 running tasks to finish:

Summary: 1 task failed:

Step 3:

embedded@embedded-HP-Z210-SFF-Workstation:~/QorIQ-SDK-V1.6-20140619-yocto/build_p2020rdb_release$ bitbake netcf -c clean

Step4:

embedded@embedded-HP-Z210-SFF-Workstation:~/QorIQ-SDK-V1.6-20140619-yocto/build_p2020rdb_release$  bitbake netcf -c patch

Step 5:

Go to netcf source in

build_p1020rdb_release/tmp/work/ppce500v2-fsl-linux-gnuspe/netcf/0.2.2+gitAUTOINC+2b0d9ca226-r1/git/.

Modify the url in the file .gitmodules as "http://repo.or.cz/r/gnulib.git"

Step 6:

. $ bitbake netcf -c configure -f

Please refer to my post on Sep 15 2014, it the detail of the steps.

After performing these 6 steps the installation stopped as shown in the post on Sep15 2014.

and when today I tried reinstalling

In the folder ~/QorIQ-SDK-V1.6-20140619-yocto/build_p2020rdb_release.

execute "source SOURCE_THIS

$ bitbake fsl-image-full

ERROR :ONly one copy of bItbake should run against build directory.

I am not able to understand whether the bitbake has been installed ???

regards

Hitu

0 件の賞賛
返信

2,553件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Hitu,

I have verified the workaround which I provided previously, it worked on my build host.

After run "bitbake netcf -c configure -f", you need to wait for a moment, because it is needed to download gnulib source code from the url "http://repo.or.cz/r/gnulib.git".

Is there problem for your host to connect to network? Is it possible to execute the command "git clone http://repo.or.cz/r/gnulib.git" on your host?

For the error "ERROR :ONly one copy of bItbake should run against build directory."

Please make sure only one bitbake building running under this folder, please close other terminal, if the error remains, please go to  folder "~/QorIQ-SDK-V1.6-20140619-yocto/" and execute the command "source ./fsl-setup-poky -m p2020rdb" again.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,553件の閲覧回数
hitusharma
Contributor II

Hi YipingI

I have reinstalled the ISO image, but while executing "bitbake fsl-image-full" I am getting this errors:

ERROR: Function failed: do_configure (log file is located at /home/embedded/QorIQ-SDK-V1.6-20140619-yocto/build_p2020rdb_release/tmp/work/ppce500v2-fsl-linux-gnuspe/netcf/0.2.2+gitAUTOINC+2b0d9ca226-r1/temp/log.do_configure.29248)

ERROR: Logfile of failure stored in: /home/embedded/QorIQ-SDK-V1.6-20140619-yocto/build_p2020rdb_release/tmp/work/ppce500v2-fsl-linux-gnuspe/netcf/0.2.2+gitAUTOINC+2b0d9ca226-r1/temp/log.do_configure.29248

ERROR: Task 3507 (/home/embedded/QorIQ-SDK-V1.6-20140619-yocto/meta-virtualization/recipes-networking/netcf/netcf_git.bb, do_configure) failed with exit code '1'How should I proceed..

regds

Hitu

0 件の賞賛
返信

2,553件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Hitu,

Please try whether the following workaround would helpful for you.

1. $ bitbake netcf -c clean

2. $ bitbake netcf -c patch

Go to netcf source in

build_p1020rdb_release/tmp/work/ppce500v2-fsl-linux-gnuspe/netcf/0.2.2+gitAUTOINC+2b0d9ca226-r1/git/.

3. Modify the url in the file .gitmodules as "http://repo.or.cz/r/gnulib.git"

4. $ bitbake netcf -c configure -f

If your problem remains, please attach the file log.do_configure.29248 to me.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,553件の閲覧回数
hitusharma
Contributor II

Hi David

The printout from lsattr fsl-setup-poky is -e

embedded@embedded-HP-Z210-SFF-Workstation:~/QorIQ-SDK-V1.6-20140619-yocto$   lsattr fsl-setup-poky

-------------e- fsl-setup-poky

how should I take it further.

regards

Hitu

0 件の賞賛
返信

2,553件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Hitu,

Please try to use the setup command like the following.

source ./fsl-setup-poky -m p1020rdb


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,553件の閲覧回数
hitusharma
Contributor II

HI Yiping

I am trying to install SDK 1.6 on Ubuntu 12.04 OS, I have installed the ISO image of QorIQ-SDK-V1.6-20140619-yocto, which created a folder in my system.I had run the script ./scripts/host-prepare.sh but while installing poky ie while running
$ source ./fsl-setup-poky -m p2020rdb
I am getting following  errors
1.
embedded@embedded-HP-Z210-SFF-Workstation:~/QorIQ-SDK-V1.6-20140619-yocto$ $ source ./fsl-setup-poky -m p2020rdb
$: command not found
2.
the file fsl-setup-poky is installed outside the sources folder so i tried running the command
mbedded@embedded-HP-Z210-SFF-Workstation:~/QorIQ-SDK-V1.6-20140619-yocto$ $  ./fsl-setup-poky -m p2020rdb
$: command not found
3.
  I tried to run the command with root privilege:
root@embedded-HP-Z210-SFF-Workstation:~/QorIQ-SDK-V1.6-20140619-yocto#  ./fsl-setup-poky -m p2020rdb
bash: ./fsl-setup-poky: Permission denied


embedded@embedded-HP-Z210-SFF-Workstation:~/QorIQ-SDK-V1.6-20140619-yocto$ source ./fsl-setup-poky -m p1020rdb

mkdir: cannot create directory `/home/embedded/QorIQ-SDK-V1.6-20140619-yocto/build_p1020rdb_release': Permission denied

kindly help me resolving the issue.

Regds

Hitu


`

0 件の賞賛
返信

2,553件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hi Hitu,

Did you install the ISO with root privilege?


Would you please let me know the result of "ls -lh fsl-setup-poky"?


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,553件の閲覧回数
hitusharma
Contributor II

Hi Yiping

Yes I did install ISO with root privilege

Plz find the result of

embedded@embedded-HP-Z210-SFF-Workstation:~/QorIQ-SDK-V1.6-20140619-yocto$ ls -lh fsl-setup-poky
-rw-r--r-- 1 554 501 16K Jun 16 08:16 fsl-setup-poky

regds

Hitu

0 件の賞賛
返信

2,553件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Hitu,

Actually you should install the ISO with normal user privilege. If you install the ISO with root privilege, other users don't have write permission in the installation folder, and only root could set up the building.

I suggest you remove this installation folder and install the ISOs again with "mbedded" user.

No need to execute host-prepare.sh again, it is enough to execute this script once.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,553件の閲覧回数
hitusharma
Contributor II

Hi Yiping

I would do that, but please le the know if I have to uninstall the exiting image manually or the new one will over right the existing one automatically?

Regds

Hitu

0 件の賞賛
返信

2,553件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Hitu,

Please under the root privilege to remove "~/QorIQ-SDK-V1.6-20140619-yocto" folder manually.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信