Hi,
I am currently using a P1024RDB .The board currently uses boot image from NOR flash. Does the P1024RDB support flashing of u-boot onto the board without a JTAG (serial or other methods if any). I want to flash my own u-boot image on the board for testing the peripherals.
Thanks.
已解决! 转到解答。
Have a great day,
U-boot itself can program NOR flash. U-boot may download image into memory, erase flash and write image to the flash. Please see
https://www.denx.de/wiki/view/DULG/UBootInstallUsingUBoot Check u-boot commands
The P1024RDB NOR flash can be split into two logical halves by setting the FBANK_SEL signal. The FBANK_SEL signal is controlled by setting SW4[8]. It also has NAND flash. So you can write your u-boot image without erasing the original.
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Have a great day,
U-boot itself can program NOR flash. U-boot may download image into memory, erase flash and write image to the flash. Please see
https://www.denx.de/wiki/view/DULG/UBootInstallUsingUBoot Check u-boot commands
The P1024RDB NOR flash can be split into two logical halves by setting the FBANK_SEL signal. The FBANK_SEL signal is controlled by setting SW4[8]. It also has NAND flash. So you can write your u-boot image without erasing the original.
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------