Does P1021 support DDR3L?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does P1021 support DDR3L?

869 次查看
rajniks
Contributor I

We are starting a design based on P1021 and wanted to know if P1021 would support DDR3L (1.35V) DDR3 memories. Please let me know if its possible.

Regards

Raj

标签 (1)
标记 (2)
0 项奖励
回复
4 回复数

675 次查看
Bulat
NXP Employee
NXP Employee

No, P1021 does not support DDR3L. Possible options are DDR2 (GVDD is 1.8V+/-90mV) and DDR3 (GVDD is 1.5V+/-75mV).

0 项奖励
回复

675 次查看
rajniks
Contributor I

Thanks for reply. Only issue is both DDR2/DDR3 don't have good life cycle and many manufacturers are obsoleting them. Hence wanted to double check as some other QorIQ series does support. Is there any part similar to P1021 with DDRL support.

0 项奖励
回复

675 次查看
Bulat
NXP Employee
NXP Employee

Try to check the datasheet of the DDR3L devices you are going to use. As far as I know, most of the DDR3L memory devices (if not all) support 1.5V supply. This means that DDR3L can be used with the P1021, however power dissipation will be higher.

675 次查看
rajniks
Contributor I

Yes I have seen on that on many devices. Thanks for the suggestion. This can be way to mitigate the lifecycle problem.

0 项奖励
回复