Hello,
There is a discrepancy about GPIO1[5] and GPIO1[15] of P1022 between its application note AN4343 and its datasheet and reference manual.
Datasheet and Reference Manual: The pin TSEC2_TX_CLK/USB2_CLK/TSEC2_GTX_CLK (Package pin number: AC26) is GPIO1_5:
Application Note (AN4343): The pin TSEC2_TX_CLK/USB2_CLK/TSEC2_GTX_CLK is GPIO1_[15]:
Reference Manual again: The pins TSEC_1588_CLK_OUT and TSEC2_TX_CLK/USB2_CLK/TSEC2_GTX_CLK are both shown as GPIO1[15] in the figure of signal groupings:
But, the pin TSEC_1588_CLK_OUT's alternate function is given as GPO1[15] two pages after the figure:
My guess is:
TSEC2_TX_CLK/USB2_CLK/TSEC2_GTX_CLK -> GPIO1[5]
TSEC_1588_CLK_OUT -> GPO1[15]
Could you confirm?
Best Regards,
Cagatay Kalelioglu
As per my personal understanding, in this case you should trust to datasheet.
I will report both these documentation issues to our documentation team and let you know the result.
Have a great day,
Alexander
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you. I'll consider datasheet is right.
You, too, have a great day.
Cagatay
I've got a confirmation, P1022 datasheet is correct.
The correct muxing on Pin# AC26 is
GPIO1_5/TSEC2_GTX_CLK/SEC2_TX_CLK/USB2_CLK.
Figure 3-1 in P1022-RM and Table 25 in P1022 design checklist - will be corrected in the next document revision.
Thank you for for pointing.
Thank you.