Hi,
We are designing a target board using p3041 CPU referring to the design of P3041DS-PC. But we have a little problem with CCSRBARH register after perform the core reset, the value is set to 0xF, so the P3041DS_init_sram.tcl cannot map entry for flash memory. We are using RCW Harded-Coded 1_0010 (16-bit NOR Flash...).
What would be the reason that this register is not set to its default value (0x0) after reset?
Thanks for any response.
Best regards.
--
Rafael
As workaround for this problem, I made the follow steps:
This solved of alternatively way, but I would like to understand by what reason the CCSRBARH is set to 0xF after PORESET.
Thanks for any response.
--
Rafael
If the P3041DS_init_sram is used the TLB entry are not valid. I think, because the script is run for CCSRBAR equal to 0x0_FE000000.
The processor is not hang, but I can not access devices mapped by script (_init_ram, for example NOR flash).
Thanks in advance.
If the CCSRBARH is changed, the P3041 MMU configuration also should be changed.
The P3041DS_init_sram.tcl file configures the 16-Mbyte region of CCSR registers to address 0x0_FE000000.
If the P3041DS_init_sram.tcl does not produce processor hanging, the CCSRBARH register value on your board is 0x0.