I am using the following:
-P1020 QorIQ processor.
-eTSEC3 (configured as eth0)
-gianfar device driver.
-Linux Kernel (Mainline Linux kernel 3.10) [NOTE: Freescale bsp 1.3 exhibits the same problem.]
-linuxptp-1.3
When running ptp4l, I get the following output:
~ # cat /bin/start_ptp4l.sh
#!/bin/sh
ptp4l -m -l 7 -i eth0 -f /etc/gPTP.cfg
~ # start_ptp4l.sh
ptp4l[39.609]: selected /dev/ptp0 as PTP clock
ptp4l[39.612]: PI servo: sync interval 1.000 kp 0.700 ki 0.300000
ptp4l[39.619]: driver changed our HWTSTAMP options
ptp4l[39.619]: tx_type 1 not 1
ptp4l[39.619]: rx_filter 1 not 12
ptp4l[39.619]: port 1: INITIALIZING to LISTENING on INITIALIZE
ptp4l[39.619]: port 0: INITIALIZING to LISTENING on INITIALIZE
ptp4l[45.619]: port 1: announce timeout
ptp4l[45.619]: port 1: LISTENING to MASTER on ANNOUNCE_RECEIPT_TIMEOUT_EXPIRES
ptp4l[45.619]: selected best master clock 000102.fffe.030405
ptp4l[45.620]: assuming the grand master role
ptp4l[45.620]: port 1: master sync timeout
ptp4l[45.622]: port 1: master sync timeout
NETDEV WATCHDOG: eth0 (fsl-gianfar): transmit queue 6 timed out
------------[ cut here ]------------
WARNING: at net/sched/sch_generic.c:255
Modules linked in: trak_fpga_itfc(O) trak_intr0(O)
CPU: 0 PID: 710 Comm: main Tainted: G O 3.10.0 #9
task: df112300 ti: c426e000 task.ti: c426e000
NIP: c040f240 LR: c040f240 CTR: c030a7b0
REGS: c426fd50 TRAP: 0700 Tainted: G O (3.10.0)
MSR: 00029000 <CE,EE,ME> CR: 22000422 XER: 20000000
GPR00: c040f240 c426fe00 df112300 0000003f 00021000 00000005 c030b15c 65756520
GPR08: 36207469 c063b11c c066f490 00000001 000000e4 1002e398 00000004 00000001
GPR16: c0584a18 c063b1c0 00400100 ffff08c1 00000000 c0635260 c0679714 ffffffff
GPR24: 00000000 00000000 00000004 00000600 c0660000 c0670000 c426e000 df022000
NIP [c040f240] dev_watchdog+0x2c4/0x2d4
LR [c040f240] dev_watchdog+0x2c4/0x2d4
Call Trace:
[c426fe00] [c040f240] dev_watchdog+0x2c4/0x2d4 (unreliable)
[c426fe40] [c00431c4] call_timer_fn.clone.26+0x28/0x80
[c426fe60] [c0043400] run_timer_softirq+0x1e4/0x1f0
[c426fea0] [c003ce04] __do_softirq+0x104/0x1c0
[c426ff00] [c003d064] irq_exit+0xa8/0xd0
[c426ff10] [c0008dc0] timer_interrupt+0x1a0/0x1cc
[c426ff40] [c000e374] ret_from_except+0x0/0x18
--- Exception: 901 at 0x100015a4
LR = 0x100015a4
Instruction dump:
4e800421 815f0204 4bfffe9c 7fe3fb78 90c10008 4bfe6edd 7fe4fb78 7c651b78
80c10008 3c60c05d 3863817c 480ee041 <0fe00000> 38000001 981c2ee0 4bffffb4
---[ end trace 6bacd068e81b67d9 ]---
ptp4l[46.953]: port 1: master sync timeout
ptp4l[48.821]: port 1: master tx announce timeout
ptp4l[48.822]: port 1: master sync timeout
ptp4l[50.821]: port 1: master sync timeout
ptp4l[52.821]: port 1: master tx announce timeout
ptp4l[52.822]: port 1: master sync timeout
ptp4l[53.690]: caught signal 2
ptp4l[53.690]: poll tx timestamp failed: Interrupted system call
ptp4l[53.690]: port 1: send sync failed
ptp4l[53.690]: port 1: MASTER to FAULTY on FAULT_DETECTED (FT_UNSPECIFIED)
ptp4l[53.690]: waiting 2^{4} seconds to clear fault on port 0
~ #
~ #
~ #
~ #
~ #
~ #
~ # ifconfig eth0
eth0 Link encap:Ethernet HWaddr 00:01:02:03:04:05
inet addr:10.80.41.229 Bcast:10.80.43.255 Mask:255.255.252.0
inet6 addr: fe80::201:2ff:fe03:405/64 Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:2976 errors:0 dropped:24 overruns:0 frame:0
TX packets:21 errors:6 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:313521 (306.1 KiB) TX bytes:1918 (1.8 KiB)
Base address:0xe000
From looking at the output one of the transmit queues timed out. Shortly thereafter the gianfar error interrupt will be called and the device driver is restarted. That happens every 2 seconds. This is killing the 1588 protocol. Does anyone have any idea as to why this is happening? I am currently trying to dig through the device driver to determine the problem, but I could use some expert advice to speed me up.
Ken
已解决! 转到解答。