Dear an Engineer in NXP
I tried to increase Output port with NXP PCAL6524, but I met a trouble.
After power-on or Reset assert sequence, I/O port (configured as an output) outputted one pulse, about 40msec.
I would like to remove the pulse, however I didn't know why the pulse appeared.
According to the datasheet 6.6, the I/O port is configured as an input.
Then the port is configured as an output by I2C command in order to modify the register set.
I have one question, is it true that the pulse about 40msec is outputted while changing the register set from Input(default) to Output?
Thanks in advance.
解決済! 解決策の投稿を見る。
Dear Yomogita-san,
please connect an oscilloscope to the I/O pin and please share the scope. By default the Output port registers are set to 1 for each pin. You can try to set the Output port register bits to 0 first and later change the input pins to output. This way the pulse should be eliminated.
Change the pins to outputs.
With Best Regards,
Jozef
Dear Yomogita-san,
please connect an oscilloscope to the I/O pin and please share the scope. By default the Output port registers are set to 1 for each pin. You can try to set the Output port register bits to 0 first and later change the input pins to output. This way the pulse should be eliminated.
Change the pins to outputs.
With Best Regards,
Jozef
Dear Jozef-san
thanks for your support.
As you said, I tried to set the register.
Then the pulse which I didn't want was disapeared.
Thank you.
Kindest Regards
Edgard