We have a I2C buffer 9511A populated on a arduino shield board, the I2C is coming from the EVK arduino header and to the buffer on arduino shield, the output of the I2C is 2.8V and to the camera module.
The current layout is the following:
what will be the proper setup?
Using this method?
Regards,
TC
Hello TC,
I hope all is great with you. Thank you for using the NXP communities.
Your configuration seems correct to me. In any case, I would recommend testing your design.
C6=0.01uF is recommended .
Please let me know if I misunderstood your question.
I hope this information helps.
Regards,
David
Hello,
Those are the maximum and minimum values for the pull-up resistor. Your design is within the range recommended.
In this case, the capacitor acts as a decoupler or filter for the power supply.
Regards,
David
how do user find out the right value instead of "within range" to use? i have 2.2K & 4.7K ohm with 0.01uF (going to try 4.7 & 4.7), this does not work. also, with 45k/45k with 0.1uF on three boards, only one work.