tag writer- password problems

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

tag writer- password problems

950件の閲覧回数
frank_fuchs
Contributor I

Hi, 

we tried to write a Tag with an "connect to WiFi" action. The tag should be protected.

Write to the tag fails every time when we add a password.

The same is for every action.

Any idea?

Frank

0 件の賞賛
返信
4 返答(返信)

719件の閲覧回数
lisettelozano
NXP Employee
NXP Employee

Hello Frank, 

Could you please provide the NXP part number? 

Paulina

0 件の賞賛
返信

719件の閲覧回数
frank_fuchs
Contributor I

Hi,

there is no part number, as I am referring to your app.

The version # is 4.4

best regards

Frank

0 件の賞賛
返信

719件の閲覧回数
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Hello Frank Fuchs,

Hope you are doing great, I think that what Paulina asked is about what tag are you using, so we can replicate te problem or explain the correct procedure in case this works for us.

BR

Jonathan

0 件の賞賛
返信

719件の閲覧回数
frank_fuchs
Contributor I

Hello,

sorry for my late reply - I've been in vacation. 

The Tag I have used is a

"NFC Sticker, 22mm, NTAG 213, 180 Bytes, white"

from the NFC-tag-shop.de 

NFC Sticker Circus, 22 mm, NTAG 213, 180 Byte, weiß | NFC Sticker weiß & schwarz | NFC Aufkleber | N... 

hope you have an idea :-)

best

Frank

0 件の賞賛
返信