s32r45's gmac default is 'rgmii' so that gmac0 tx clock is currently output.
We should change tx clock as input in order to use 'mii'
Accordingly, s32r45-pinctrl.h file has been changed as follow
In T32, modification above is not applied to register
Any advice?
已解决! 转到解答。
Hi Eddy,
I just tried this out on BSP32 and it seems to work:
The change you made is exactly the one I did on Uboot:
diff --git a/include/dt-bindings/pinctrl/s32r45-pinctrl.h b/include/dt-bindings/pinctrl/s32r45-pinctrl.h
index 3a80e52925..5c60a6f030 100644
--- a/include/dt-bindings/pinctrl/s32r45-pinctrl.h
+++ b/include/dt-bindings/pinctrl/s32r45-pinctrl.h
@@ -251,7 +251,7 @@
/* PE02 */
#define PE02_MSCR_S32R45 (66)
#define PE02_GMAC0_TX_CLK_CFG (SIUL2_MSCR_S32_G1_MUX_ID_1 | \
- ENET_CLK_PIN_CFG)
+ ENET_IN_PIN_CFG)
#define PE02_GMAC0_TX_CLK_IN (SIUL2_MSCR_S32_G1_MUX_ID_2)
/* PE03 */
make s32r45evb_defconfig
make CROSS_COMPILE=/<To toolchain path>/gcc-arm-10.2-2020.11-x86_64-aarch64-none-linux-gnu/bin/aarch64-none-linux-gnu-
make CROSS_COMPILE=/<To toolchain path>/gcc-arm-10.2-2020.11-x86_64-aarch64-none-linux-gnu/bin/aarch64-none-linux-gnu- ARCH=aarch64 PLAT=s32r45evb BL33=/<To Uboot Path>/u-boot/u-boot-s32.bin
sudo dd if=fip.s32 of=/dev/mmcblk0 skip=512 seek=512 iflag=skip_bytes oflag=seek_bytes conv=fsync,notrunc
If you are following these steps it is likely that the image is not being updated.
Saludos,
Alejandro
Hi Eddy,
I just tried this out on BSP32 and it seems to work:
The change you made is exactly the one I did on Uboot:
diff --git a/include/dt-bindings/pinctrl/s32r45-pinctrl.h b/include/dt-bindings/pinctrl/s32r45-pinctrl.h
index 3a80e52925..5c60a6f030 100644
--- a/include/dt-bindings/pinctrl/s32r45-pinctrl.h
+++ b/include/dt-bindings/pinctrl/s32r45-pinctrl.h
@@ -251,7 +251,7 @@
/* PE02 */
#define PE02_MSCR_S32R45 (66)
#define PE02_GMAC0_TX_CLK_CFG (SIUL2_MSCR_S32_G1_MUX_ID_1 | \
- ENET_CLK_PIN_CFG)
+ ENET_IN_PIN_CFG)
#define PE02_GMAC0_TX_CLK_IN (SIUL2_MSCR_S32_G1_MUX_ID_2)
/* PE03 */
make s32r45evb_defconfig
make CROSS_COMPILE=/<To toolchain path>/gcc-arm-10.2-2020.11-x86_64-aarch64-none-linux-gnu/bin/aarch64-none-linux-gnu-
make CROSS_COMPILE=/<To toolchain path>/gcc-arm-10.2-2020.11-x86_64-aarch64-none-linux-gnu/bin/aarch64-none-linux-gnu- ARCH=aarch64 PLAT=s32r45evb BL33=/<To Uboot Path>/u-boot/u-boot-s32.bin
sudo dd if=fip.s32 of=/dev/mmcblk0 skip=512 seek=512 iflag=skip_bytes oflag=seek_bytes conv=fsync,notrunc
If you are following these steps it is likely that the image is not being updated.
Saludos,
Alejandro