read the program of the chip through JTAG

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

read the program of the chip through JTAG

770件の閲覧回数
bin_wang
Contributor I

The chip chosen by the customer is MC56F82723. Is there any method to read the program of the chip through JTAG?

ラベル(1)
  • DSC

0 件の賞賛
1 返信

739件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, WangBin,

Yes, you can download the Flash programming tools from the link:

PROGDSC | Flash/EEPROM Programmer Software for DSC devices | PEmicro 

With the tools and MultiLink Universal device, you can read code or data  and program the on-chip flash of MC56F82xxx.

The MC56F82xxx supports the flash security function, when you write a specific byte to a specific address of flash, the JTAG is blocked to protect cusomer IP.

Hope it can help you

BR

XiangJun Rong

0 件の賞賛