"L'initialisation du TED-Kit 2 avec le numéro de série "AH035YWX" a échoué. Ce TED-Kit 2box ne peut

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

"L'initialisation du TED-Kit 2 avec le numéro de série "AH035YWX" a échoué. Ce TED-Kit 2box ne peut

13,554件の閲覧回数
mednassim
Contributor I
 
0 件の賞賛
返信
15 返答(返信)

13,532件の閲覧回数
mednassim
Contributor I

I accidentally clicked "debug TED-kit", then it can't connect to TED-kit2 tool. How to fix this problem? (initialisation of ted-kit 2 with serial number "ah035ywx" failed. this tedkit 2 box cannot be used and is not shown in the hardware view.)

0 件の賞賛
返信

12,716件の閲覧回数
wxf5555
Contributor I

I can fix it

0 件の賞賛
返信

13,538件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello @mednassim .

In order to better service for you. Would you please kindly describe your detail information in English?

 

Have a nice day!

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 件の賞賛
返信

13,528件の閲覧回数
mednassim
Contributor I

hello @fangfang 

I accidentally clicked "debug TED-kit", then it can't connect to TED-kit2 tool. How to fix this problem? (initialisation of ted-kit 2 with serial number "ah035ywx" failed. this tedkit 2 box cannot be used and is not shown in the hardware view.)

0 件の賞賛
返信

13,496件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello @mednassim 

Thanks for your information.

For the TED-Kit2 problem you could reinstalled the software and tested it again.

Hope it help you.

 

 

タグ(1)
0 件の賞賛
返信

13,071件の閲覧回数
shrikant_koli
Contributor I

In my case this same issue is came.

@fangfang whichever solution you had provide like reinstall the software.

but still its not working.

If you have any solution please provide us.

please find attachment for your reference.

0 件の賞賛
返信

13,486件の閲覧回数
mednassim
Contributor I

Hello,


Thanks for your help
But the problem of x86 processor error message appears during installation

0 件の賞賛
返信

13,530件の閲覧回数
mednassim
Contributor I

I accidentally clicked "debug TED-kit", then it can't connect to TED-kit2 tool. How to fix this problem? (initialisation of ted-kit 2 with serial number "ah035ywx" failed. this tedkit 2 box cannot be used and is not shown in the hardware view.)

0 件の賞賛
返信

12,715件の閲覧回数
wxf5555
Contributor I
I can fix it
0 件の賞賛
返信

12,573件の閲覧回数
32mao
Contributor I

怎样修复

0 件の賞賛
返信

12,537件の閲覧回数
wxf5555
Contributor I

我的邮箱:wxf-5555@163.com,我在苏州

0 件の賞賛
返信

12,539件の閲覧回数
wxf5555
Contributor I

你在哪边?方便把东西寄过来处理吗?

0 件の賞賛
返信

12,535件の閲覧回数
32mao
Contributor I

已经解决了,谢谢你。可以把盒子拆掉,里面板子有J-LINK接口,我是通过J-LINK接口然后把firmware文件里的十六进制文件给烧录进去的,然后就没问题了。

0 件の賞賛
返信

12,526件の閲覧回数
wxf5555
Contributor I

在自动测试和生产方面,我们有研发自己的读写器和相关LABVIEW驱动,

0 件の賞賛
返信

12,531件の閲覧回数
wxf5555
Contributor I

对的,是这样的!你们是用在哪方面了?

0 件の賞賛
返信