p2020 rdb

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

p2020 rdb

Jump to solution
2,341 Views
eagles
Contributor I

What's included with the board purchase? Do I get USB Tap and limited edition of code warrior? Am I able to open box and do some programming?

Thanks in advance.

0 Kudos
1 Solution
590 Views
Joe2010
Contributor I

Hi

The list of deliverables include:

 

1. USB TAP

2. Limited edition Codewarrior

3. BSP CD for the P2020 RDB

4. The board comes with U-boot preinstalled.

 

You can load the linux image thru USB, NOR, NAND or NFS.

 

Yes you can do some programming out of box.

 

 

View solution in original post

0 Kudos
2 Replies
591 Views
Joe2010
Contributor I

Hi

The list of deliverables include:

 

1. USB TAP

2. Limited edition Codewarrior

3. BSP CD for the P2020 RDB

4. The board comes with U-boot preinstalled.

 

You can load the linux image thru USB, NOR, NAND or NFS.

 

Yes you can do some programming out of box.

 

 

0 Kudos
590 Views
eagles
Contributor I

Thank you very much.

0 Kudos