inconsistent performance of the BFU790F

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

inconsistent performance of the BFU790F

560 次查看
pragashsangaran
Contributor I

we have been using BFU790F for our design since 2019. the weird thing we noticed is the board to board variation is too much. our LNA cant get consistent performance at all. did anyone see this problem? is this a known problem which has been fixed recently?

0 项奖励
2 回复数

536 次查看
andrei_skok
NXP Employee
NXP Employee

We are not aware about any problem with the BFU790F that would cause any performance degradation. Please note, the board performance may depend not only on the BFU790F itself but also on other components and your hardware design. We suggest our customers to go through one of our dedicated RF distributors such as Richardson RFPD and RFMW. We rely on their support for these types of inquiries as they would become more involved in the full design of the product.

0 项奖励

523 次查看
pragashsangaran
Contributor I

we are using BFU790F, and im trying to impedance match BFU790F to 50ohm to design LNA. could you please give me the input impedance and output impedance of the BFU790F and the gain, output power, NF, and other parameters at that impedance? basically, I'm asking for the results of the load-pull measurement. 

 

BR

pragash

0 项奖励